RT1024 Interface with FRDM-LVPMSM daughter board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1024 Interface with FRDM-LVPMSM daughter board

831 次查看
Krish403
Contributor I

Hi,

I am using MIMXRT1024 EVK with FRDM-MCLVPMSM daughter board. Stacking together as the form factor for both boards are matching and the net names also matching. 

My aim is to spin the Linix and Teknic motors using the mc_pmsm demo project. But I am unable to spin it. If spins, it's intermittent.

Here are my questions: 

1) Can I stack the RT1024 and FRDM-MCLVPMSM board? Is there any wiring diagram for both the boards?

2) Is there any document to use RT1024 (not RT1020, bcz connectors and some connections are different) and FRDM-LVPMSM? If so please attach.

3) If I wanted to spin the motor, do I need to do any modifications( adding/removing any resistors) for the RT1024 EVK board?

4) Is Rev.Code- B1 is the latest schematics?

Krish403_0-1634854509394.png

5) Is there any wiring details for LINIX motor?

Please answer the above questions.

Thank you.

 

 

 

 

 

0 项奖励
1 回复

813 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Please see my answers below:

1,2,3,5) Please check application user's guide attached.

4) Yes, this is latest version.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

0 项奖励