RT1021 ENC Driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RT1021 ENC Driver

跳至解决方案
1,906 次查看
kaangencay
Contributor I

Hi all,

I am using RT1021 MCU and I want to implement ENC driver. 

When I check the fsl_enc.c driver code, I realized that ENC_GetPositionValue() function returns UPOS and LPOSH and also ENC_GetHoldPositionValue() function returns UPOSH and LPOSH.  I think ENC_GetPositionValue() should return UPOS and LPOS registers' value.

I am using;
MCUXpresso IDE
SDK_2.x_EVK-MIMXRT1020
SDK Version: 2.11.0
Manifest Version 3.9.0
enc dirver version: 2.1.0

Is there any mistake or am I wrong?

标签 (1)
0 项奖励
1 解答
1,883 次查看
jay_heng
NXP Employee
NXP Employee

Yes, it is driver issue, i have created ticket for it and assign it to dev team. thanks

This issue should be fixed in v2.1.1 or v2.2

在原帖中查看解决方案

0 项奖励
1 回复
1,884 次查看
jay_heng
NXP Employee
NXP Employee

Yes, it is driver issue, i have created ticket for it and assign it to dev team. thanks

This issue should be fixed in v2.1.1 or v2.2

0 项奖励