RT1020: How long is a wait state (e.g. GPIO, GPT peripherals)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1020: How long is a wait state (e.g. GPIO, GPT peripherals)?

764 次查看
rshipman
Contributor V

Hi,

Regarding document:

i.MX RT1020 Processor Reference Manual, Rev. 1, 12/2018

What does it mean by a wait state? Is this a single cycle of the peripheral’s root clock, the periph clock, processor clock, a __NOP() or what?

E.g. the GPIO peripheral:

Section 11.5.2.2, page 786

Section 11.5.4.2, page 789

Section 11.5.8.2, page 799

E.g. the GPT peripheral:

Section 46.7 GPT Memory Map/Register Definition, page 2451

Section 46.7.1 GPT Control Register (GPTx_CR), page 2453

There are other references to the wait state.

Many thanks and regards,

Ronnie

标签 (1)
0 项奖励
2 回复数

697 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the information as the it.

 

pastedImage_1.png

 Hope it  help you. Have a nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 项奖励

697 次查看
rshipman
Contributor V

Thank you for your reply.

Unfortunately, I'm not sure that answers my question. Perhaps my question was a bit clumsy.

When the document talks about wait states, I understand that it is in terms of clocks cycles. I.e. one wait state = one clock cycle.

But which clock? Is it the the main processor clock? Or is it the root clock to the peripheral in question? Please see the sections I mentioned.

Kind regards,

Ronnie

0 项奖励