RT1015 BEE XIP protect region

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1015 BEE XIP protect region

Jump to solution
658 Views
kensu
Contributor V

Hi,

https://www.itdaan.com/tw/6ee145c52115d5b35c15c55160da6864 

The BEE XIP can set two region.

Each region can set Start Address and Length.

I want to know how MCU know this information?

In the image header?

pastedImage_2.png

Regards

Ken

Labels (1)
1 Solution
617 Views
jeremyzhou
NXP Employee
NXP Employee

Hi

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
1) I want to know how MCU knows this information? In the image header?
-- The encrypted protection region descriptor block is included in the Image Vector Table, you can learn it from the section: 2.4.2. Image layout & encrypt XIP flow in the application note: AN12079.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
618 Views
jeremyzhou
NXP Employee
NXP Employee

Hi

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
1) I want to know how MCU knows this information? In the image header?
-- The encrypted protection region descriptor block is included in the Image Vector Table, you can learn it from the section: 2.4.2. Image layout & encrypt XIP flow in the application note: AN12079.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------