RT1011 W25Q256 FLM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1011 W25Q256 FLM

Jump to solution
928 Views
Daniel14
Contributor III

Hi, 

MIMXRT1011 official demo use AT25SF128A-SHB-T as flash however I use W25Q256JV instead. My code run well when debug but failed to run when I load the code to flash using default FLM file. I thought the issue may cause from the wrong FLM file.

Do you have FLM file that suitable for W25Q256JV? or how can I generate FLM file?

Thanks. 

0 Kudos
1 Solution
903 Views
jay_heng
NXP Employee
NXP Employee

See detailed usage of RT-UFL under MDK (It is in chinese)

超级下载算法RT-UFL v1.0在Keil MDK下的使用

View solution in original post

0 Kudos
7 Replies
842 Views
Daniel14
Contributor III

Thanks for your support.

0 Kudos
914 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest support, I'd like to suggest you refer to the open-source project.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------

0 Kudos
910 Views
Daniel14
Contributor III

Hi, Jeremy

Thanks a lot for your fast response. I just tried it. Modified the FlashDev.c  that below. then generate FLM. 


// MIMXRT1010-EVK

struct FlashDevice const FlashDevice = {
FLASH_DRV_VERS, // Driver Version, do not modify!
"MIMXRT_FLEXSPI", // Device Name
EXTSPI, // Device Type
0x60000000, // Device Start Address
// 0x01000000, // Device Size in Bytes (16mB)
0x02000000, // Device Size in Bytes (32mB)
256, // Programming Page Size
0, // Reserved, must be 0
0xFF, // Initial Content of Erased Memory
100, // Program Page Timeout 100 mSec
5000, // Erase Sector Timeout 5000 mSec

// Specify Size and Address of Sectors
0x1000, 0x00000000, // Sector Size 4kB (256 Sectors)
SECTOR_END
};

 

Load the code on my board. Output show "Insufficient RAM for Flash Algorithms !" like below.

Load "flexspi_nor_release\\igpio_led_output.out"
Insufficient RAM for Flash Algorithms !
Erase Failed!
Error: Flash Download failed - "Cortex-M7"
Flash Load finished at 16:58:44

 

then I modify the RAM for Algorithm Size from 0x8000 to 0x16000 and they again.

Output shows Cannot access memory.

BTW, I use default .scf file without any modification.

Thanks. 

 

Daniel14_0-1666170307901.png

Daniel14_1-1666170390762.png

 

 

0 Kudos
909 Views
Daniel14
Contributor III

This is pop-up window when I load the code after modifying the size

Daniel14_0-1666171002342.png

 

0 Kudos
904 Views
jay_heng
NXP Employee
NXP Employee

See detailed usage of RT-UFL under MDK (It is in chinese)

超级下载算法RT-UFL v1.0在Keil MDK下的使用

0 Kudos
894 Views
Daniel14
Contributor III

Hi.Jay

Thanks, It seems only support Jlink but not DAP link?

0 Kudos
859 Views
jay_heng
NXP Employee
NXP Employee

Yes, currently it supports Jlink only

0 Kudos