Hi All
This is the QSPI flash configuration as used for booting the iMXRT1064 EVK:
const flexspi_nor_config_t qspiflash_config = {
.memConfig =
{
.tag = FLEXSPI_CFG_BLK_TAG,
.version = FLEXSPI_CFG_BLK_VERSION,
.readSampleClkSrc = kFlexSPIReadSampleClk_LoopbackFromDqsPad,
.csHoldTime = 3u,
.csSetupTime = 3u,
// Enable DDR mode, Wordaddassable, Safe configuration, Differential clock
.sflashPadType = kSerialFlash_4Pads,
.serialClkFreq = kFlexSpiSerialClk_100MHz,
.sflashA1Size = 8u * 1024u * 1024u,
.lookupTable =
{
// Read LUTs
FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x18),
FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, 0x06, READ_SDR, FLEXSPI_4PAD, 0x04),
},
},
.pageSize = 256u,
.sectorSize = 4u * 1024u,
.blockSize = 256u * 1024u,
.isUniformBlockSize = false,
};
As far as I have understood the chip boots from its internal 4MB QSPI flash chip (on FlexSPI2 and at 0x70000000) but there are two entries in the table that I don't understand:
1.
.sflashA1Size = 8u * 1024u * 1024u,
Should this not be 4M and not 8M?
2.
.blockSize = 256u * 1024u,
The internal QSPI flash (W25Q32JV) has 64k block size and not 256k block size?
Are these entries incorrect but on non-importance or is there another explanation?
Regards
Mark
Hi Mark,
Thanks for reporting this! I already reported it with the SDK team and this will be fixed in future releases. As long as you don't use a flash size greater than 4MB you won't get any issues with this configuration.
Regards,
Victor
Hi Mark,
The block size is consistent with flash size, you can look at them as one parameter and it only impacts the register FLASHA1CR0. This will only cause a problem when the desired access flash address is more than the actual flash size (4MB).
Regards,
Victor