Good day All,
I have imported the RT1021's SDK lwip_udpecho_bm example and this works fine with the original settings (e.g Flash and SRAM_DTC). However, as I added more functionality I ran out of DTC ram and so I modified the project mcu settings such that the SRAM_OCRAM was used (e.g. moved SRAM_OCRAM up in the MCU Settings). The application compiled fine and revealed that indeed the OCRAM was being used:
Memory region Used Size Region Size %age Used
BOARD_FLASH: 95888 B 8 MB 1.14%
SRAM_OC: 62528 B 128 KB 47.71%
SRAM_DTC: 88 B 64 KB 0.13%
SRAM_ITC: 0 GB 64 KB 0.00%
BOARD_SDRAM: 0 GB 32 MB 0.00%
Finished building target: evkmimxrt1020_lwip_udpecho_bm.axf
When I rerun the application it does not respond to UDP packets. if I ping the target most times the pings do not respond and if they do it only responds to 2 pings and then no more.
Before I start digging into this further I thought I would ask to see if anyone has come across this issue and why does it only become a problem when OCRAM is used?
Thanks in advance!
Cheers,
Sam
解決済! 解決策の投稿を見る。
Good day All,
I reviewed the same FreeRtos version of the bm example (evkmimxrt1020_lwip_udpecho_freertos) and here I found some examples of where caching is needed and/or disabled in order to have lwip working. As a consequence I will use this example as a reference for I need and so I think this answered my question
Cheers,
Sam
Hi samsaprunoff :
In cases you are using OCRAM as your main RAM, For LwIP I would suggest you put some key data structures to SRAM_DTC or other non-cacheable region.
Regards
Daniel
Good day Daniel,
Thank you for your response!
There is some data that is already being stored in DTC, as indicated by the compile results:
Memory region Used Size Region Size %age Used
BOARD_FLASH: 95888 B 8 MB 1.14%
SRAM_OC: 62528 B 128 KB 47.71%
SRAM_DTC: 88 B 64 KB 0.13%
SRAM_ITC: 0 GB 64 KB 0.00%
BOARD_SDRAM: 0 GB 32 MB 0.00%
Finished building target: evkmimxrt1020_lwip_udpecho_bm.axf
Would you have any suggestions as to what other lwip data needs to be stored in DTC?
Cheers,
Sam
ENET buffers need to store in SRAM_DTC
Original definition:(enet_ethernetif_kinetis.c)
SDK_ALIGN(static rx_buffer_t rxDataBuff_0[ENET_RXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);
SDK_ALIGN(static tx_buffer_t txDataBuff_0[ENET_TXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);
Change to:
AT_NONCACHEABLE_SECTION_ALIGN(static rx_buffer_t rxDataBuff_0[ENET_RXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);
AT_NONCACHEABLE_SECTION_ALIGN(static tx_buffer_t txDataBuff_0[ENET_TXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);
Regards
Daniel
Good day Daniel,
Excellent, thank you for this great info!
Cheers,
Sam
Good day All,
I reviewed the same FreeRtos version of the bm example (evkmimxrt1020_lwip_udpecho_freertos) and here I found some examples of where caching is needed and/or disabled in order to have lwip working. As a consequence I will use this example as a reference for I need and so I think this answered my question
Cheers,
Sam