Precision of NVCC_PLL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Precision of NVCC_PLL

603 Views
chenfei_203
Contributor I

Hi all.

I want to use a 24M oscillator(3.3V) to connect to XTALO. But the logic level of this forcing clock must not exceed the NVCC_PLL level(Typical Programming Operating Range is 1.0V to 1.2 V with the nominal default setting as 1.1 V). 

My question is whether i can use two resistances to divide the output of oscillator to satisfy the requirement of XTALO DC parameters.And the precision of NVCC_PLL.

Tags (2)
0 Kudos
1 Reply

554 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

 

This has not been tested but it looks like it could work. Please just take into considerations that 'the crystal must be rated for a maximum drive level of 250 uW as it is stated in datasheet.

 

Best regards,

Felipe

0 Kudos