Hi everyone,
An RT106x board with SDRAM I've been asked to look at has been designed to use EMC_39 as a spare GPIO. Reading the Reference Manual, it seems the way to configure the registers for this would be to set DQSMD = 0 (in the SEMC_MCR register) and then set up the ALT5 pinmux for EMC_39.
However, even though the SDRAM currently works fine with DQSMD = 1, the moment I set DQSMD to 0 the SDRAM stops working (and this is in EMC_39's ALT0 pinmux mode, never mind the ALT5 mode).
My best guess is that the SEMC timings for the SDRAM would need to be edited in order to get DQSMD = 0 working, but I think I'm missing some key information to achieve this.
What would I need to do to get DQSMD = 0 this working? Is DQSMD = 0 (disabled) much slower than DQSMD = 1 (enabled)?
All hints and suggestions gratefully received!
Thanks, Nick
PS: the two closest posts I found were this RT1050 one from 2019 by David Rodgers ( @dmarks_ls
https://community.nxp.com/t5/i-MX-RT/RT1050-Can-SDRAM-DQS-be-looped-back-internally/m-p/907390
...and this RT1020 post from 2020 by Ronnie Shipman ( @rshipman
https://community.nxp.com/t5/i-MX-RT/RT1020-clocking-SDRAM-at-166Mhz-Zero-timing-margin/m-p/1039370
解決済! 解決策の投稿を見る。
Hi
In order to move from DQSMD 1 to DQSMD 0 you must (first) reduce the SEMC_CLK_ROOT speed to about 60MHz.
From the data sheet it is seen that 133/166MHz speed is not supported when using the alternative configuration:
See pages 20..21 of https://www.utasker.com/docs/iMX/i.MX_RT_1021_uTasker.pdf for SEMC clock settings and check how it is set as default (eg. via DCD) then increase the root divide value (SEMC_PODF) in CCM_CBCDR accordingly.
This can either be done generally in the DCD or else the DCD can be set for full speed and then the change be made on-the-fly when the GPIO is needed - note however that the pin should usually be left floating for the highest speed of operation ad not connected to external circuitry.
Regards
Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or rapid product development requirements
For professionals searching for faster, problem-free Kinetis and i.MX RT 10xx developments the uTasker project holds the key: https://www.utasker.com/iMX/RT1060.html
Note #1: I know that the DQSMD setting is editable via the SEMC configuration structure in the SEMC peripheral, i.e. Dummy read strobe mode = "Dummy read strobe loopbacked internally". But I don't know how to recalculate the SDRAM configuration settings to make it actually work.
Note #2: it seems @mjbcswitzerland may have attempted something along these lines, as per:
Hi
In order to move from DQSMD 1 to DQSMD 0 you must (first) reduce the SEMC_CLK_ROOT speed to about 60MHz.
From the data sheet it is seen that 133/166MHz speed is not supported when using the alternative configuration:
See pages 20..21 of https://www.utasker.com/docs/iMX/i.MX_RT_1021_uTasker.pdf for SEMC clock settings and check how it is set as default (eg. via DCD) then increase the root divide value (SEMC_PODF) in CCM_CBCDR accordingly.
This can either be done generally in the DCD or else the DCD can be set for full speed and then the change be made on-the-fly when the GPIO is needed - note however that the pin should usually be left floating for the highest speed of operation ad not connected to external circuitry.
Regards
Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or rapid product development requirements
For professionals searching for faster, problem-free Kinetis and i.MX RT 10xx developments the uTasker project holds the key: https://www.utasker.com/iMX/RT1060.html