I'm looking to achieve the fastest possible graphics, i.e. scrolling, animations, etc... on the iMX RT1176, running in landscape 720x1280. What settings / example LVGL demo could I reference? Right now I'm using the MIMXRT1170-EVKB and RK055HDMIPI4MA0 5.5" inch screen.
Also using FreeRTOS, not bare metal...
Thank you,
Scott
解決済! 解決策の投稿を見る。
Hi @application_ninja ,
The original example report 20FPS on my board. If you set compile optimization level to -O2, it will be 34FPS.
The example use VGLite to off-load CPU work load. If you set LV_USE_GPU_NXP_VG_LITE to 0, the weighted FPS is 24. And if you set compile optimization to -O2, it will be 47FPS.
Regards,
Jing
Hi @application_ninja ,
Please use GUI Guider. It's base on LVGL and is optimized for RT1176 and PXP.
https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER
Regards,
Jing
I have tried GUI Guider and the results are still slow, this is why I am asking what are the optimal settings that can be used to achieve the best results? I would think a dual core 1Ghz processor should produce lighting fast graphics, but that's just not the case. Running the example "benchmark" LVGL programs result in less than 15fps, is this normal / expected?
Hi @application_ninja ,
The original example report 20FPS on my board. If you set compile optimization level to -O2, it will be 34FPS.
The example use VGLite to off-load CPU work load. If you set LV_USE_GPU_NXP_VG_LITE to 0, the weighted FPS is 24. And if you set compile optimization to -O2, it will be 47FPS.
Regards,
Jing
-O2 does help, but still not the performance I'd expect from this device.