Need MQTT for AWS IOT application on IMX RT1170

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need MQTT for AWS IOT application on IMX RT1170

722 次查看
fmabrouk
Contributor III

I Need to use MQTT for AWS IOT application on IMX RT1170. Is there any demo code for this to get me started. Otherwise, does IMX RT1060 comes with an MQTT demo code?

0 项奖励
1 回复

704 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Unfortunately, since the RT1170 is still in pre-production, you will need to contact your local NXP representative to discuss any information related to this device. I apologize for the inconvenience that this might cause you. 

Regarding your second question, the i.MX RT1060 SDK comes with the lwip_mqtt_freertos example for your reference.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 项奖励