NAND FLASH XIP and boot modes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND FLASH XIP and boot modes

ソリューションへジャンプ
1,642件の閲覧回数
ahmedhrabi
Contributor III

Hi all, 

I'am working on the IMXRT1176 and i have some questions about the memory usage : 

  1. Did the XIP support NAND flash through QSPI?
  2. If the IMXRT1170 boot from NAND flash, then the loader must copy the application to external or internal SDRAM. Our application will for sure exceed the OCRAM, so it will be copied to the external SDRAM, so is the debug functionnal for an application that is copied from NAND falsh to SDRAM?
  3. Is there any SDK example for that use?
  4. Can i split the NAND flash on two partitions :
    • First partition for the application code
    • Second partition will be formatted as FAT32 file system

Regards, 

HRABI.

0 件の賞賛
1 解決策
1,618件の閲覧回数
jay_heng
NXP Employee
NXP Employee

1. You can refer to System Boot chapter in Reference Manual for more detail of BootROM

2. You can debug application in SDRAM by debugger directly, SDRAM init work will be done by debugger/IDE script. in this case, application cannot boot after power-up

元の投稿で解決策を見る

4 返答(返信)
1,623件の閲覧回数
ahmedhrabi
Contributor III

@jay_heng

Thank you for this responses, can you please give me more informations about thus two points : 

  • I'am a little bit confused about the BootROM, it is an accessible application and how can i modify it to copy the user aplication from NAND to external SDRAM? Is there any example of BootROM application? 
  • For the 3rd point, If I have understood correctly, i canno't debug the image application. And i have absolutly to use the MCUbootUtility to download the image on NAND Flash, is this true? 

Regards, 

HRABI.

 

 

0 件の賞賛
1,619件の閲覧回数
jay_heng
NXP Employee
NXP Employee

1. You can refer to System Boot chapter in Reference Manual for more detail of BootROM

2. You can debug application in SDRAM by debugger directly, SDRAM init work will be done by debugger/IDE script. in this case, application cannot boot after power-up

1,629件の閲覧回数
jay_heng
NXP Employee
NXP Employee

1. NAND device cannot support XIP feature.

2. BootROM will help to copy your image from NAND to SDRAM, then boot application. For SDRAM init, you need to enable DCD.

3. You can refer to below SDK demo (sdram_text debug build), but need to modify linker file for boot. and flash this image by MCUBootUtility

\SDK_2.11.1_MIMXRT1170-EVK\boards\evkmimxrt1170\demo_apps\hello_world

1176_SDRAM.PNG

4. Yes, you can.

910件の閲覧回数
pguan
Contributor I

1) According to the requirements,I modified the SCF file according to following

#define m_interrupts_start 0x80002000
#define m_interrupts_size 0x000023FF

#define m_text_start 0x80002400
#define m_text_size 0x001FFFFF

2) And add the following to marco.

XIP_BOOT_HEADER_ENABLE=1,

XIP_BOOT_HE

 

ADER_DCD_ENABLE=1

3)  Generate the image.

4)  Using the NXP-MCUBootUtility  to download the iamge.

     DEV UNSIGNED IMAGE BOOT. 

5)  Cannot run. ( but MDK debug is OK.) 

0 件の賞賛