MiMxRT1020 lpi2c clock is not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MiMxRT1020 lpi2c clock is not working

1,020 Views
meeras
Contributor I

I am using SDK_2.7.0_EVK_MIMXRT1020.zip  example code evkmimxrt1020_lpi2c_polling_b2b_master , but the problem is clock is  not generating for this example code. I checked with logic analyzer. Please help me with this.

Labels (1)
Tags (2)
0 Kudos
3 Replies

959 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

I just ran the example evkmimxrt1020_lpi2c_polling_b2b_master and evkmimxrt1020_lpi2c_polling_b2b_slave with two RT1020 EVKs and I didn't find any errors. In which pin are you trying to see the  I2C clock signal? 

Regards, 

Victor 

0 Kudos

959 Views
meeras
Contributor I
    Thanks for answering my question. GPIO_AD_B1_14 is configured as LPI2C1_SCL and GPIO_AD_B1_15 is configured as LPI2C1_SDA. Connector j19 7th line is connected to GND and 8th line is connected to VCC.
0 Kudos

959 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Thanks for the reply! You don't need to connect anything to J19-8, this pin is internally connected to 3.3V. Could you please confirm that you are trying to see the clock signal on the pin J18-6? What are you using as a slave? 

Regards, 

Victor 

0 Kudos