Max Clock Frequency of HyperRAM memory for RT1172

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Max Clock Frequency of HyperRAM memory for RT1172

Jump to solution
442 Views
LuisC
Contributor II

Hello,

 

On table 10-48 of the reference manual, I see that the max clock frequency for serial RAM is dependent on the chip. However, in other documentation I see that the max clock frequency for the FlexSPI peripheral is 166 MHz.

We are planning to use a HyperRAM chip that has a max clock frequency of 250 MHz. Will this clock speed by obtainable through FlexSPI, does the 166 MHz boundary only apply to Flash?

 

0 Kudos
Reply
1 Solution
414 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @LuisC ,

No, this restriction apply to all the device interface with FlexSPI. 250M is impossible.

 

Regards,

Jing

View solution in original post

1 Reply
415 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @LuisC ,

No, this restriction apply to all the device interface with FlexSPI. 250M is impossible.

 

Regards,

Jing