Dears,
I got stuck at MIMXRT685-EVK Debug, while I following the Getting Start with XPlorer for RT600.pdf, J-Link runs normal, and XPlorer cannot process.
When configured debug and connecting, it appears as below,
I Clicked OK, it report below error,
Clicked OK, then,
Can you please kindly help to advice?
Thanks & BRs,
Ray
Hi Ray Deng
When you build the DSP project, do you meet any build issues?
This is my situation:
Tomorrow, I do more test about it.
Best Regards,
Kerry
Hi Kerry,
Yes, it is the error reported from Makefile,
BRs,
Ray
Hi Ray Deng,
I just ignore the errors, and debug the code, I can enter the debug mode:
But, before I download the DSP code, I have downloaded the ARM core code, and run it, then debug the DSP code.
This is the printf information:
The xt-ocd.exe -c topology.xml information is also the same as you!
Do you download the ARM core at first with the MCUXPresso IDE?
Best Regards,
Kerry
Hi Ray Deng ,
Please tell me which XPlorer IDE version you are using now? Xplore IDE 8.0.10?
Do you also refer to chapter 1.5 Install Xtensa On Chip Debugger Daemon, please make sure you really do it step by step following the document.
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Kerry,
Thanks for your kindly help,
I DO following the steps that Getting Started with Xplorer for RT600.pdf. My Xplorer version is 8.0.10.
BRs,
Ray
Hi Ray Deng
Thanks for your information.
I will do it on my side, please give me more time.
Any updated information, I will let you know ASAP, please keep patient, thanks.
Best Regards,
Kerry