[MIMXRT685-AUD-EVK] 'xtensa_read_memory' failed on Xtensa OCD Daemon

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MIMXRT685-AUD-EVK] 'xtensa_read_memory' failed on Xtensa OCD Daemon

2,200 Views
gnani
Contributor I

Hi all.

I'm trying to debug MIMXRT685-AUD-EVK board for using customized voip library.

So I added customized voip library(about 920KB) to \devices\MIMXRT685S\xtensa\gdbio\ folder

and some DSP codes to xa-capturer-dmic.c's xa_hw_capturer_read_FIFO().

Debug and run on Xtensa Xplorer IDE, I can see error message on xt-ocd daemon window like below.

 

Spoiler
Error: Exception!
Error: Exception details: exccause:0xd, excvaddr:0x428a0038, epc:0x1cfe04, epcdbg:2402063c
Error: Op 'xtensa_read_memory' failed, will not retry
ERROR: Command 'm428a0038,4' failed!
Error: Exception!
Error: Exception details: exccause:0xd, excvaddr:0x428a0038, epc:0x240205bc, epcdbg:2402063c
Error: Op 'xtensa_read_memory' failed, will not retry
ERROR: Command 'm428a0038,4' failed!
Error: Exception!
Error: Exception details: exccause:0xd, excvaddr:0x428a0030, epc:0x240205bc, epcdbg:2402063c

 

 

<Development Enviroment>

PC: window 10

EVK: MIMXRT685-AUD-EVK

SDK: dsp_xaf_record_hifi4

MCUXpresso v11.5.1

Xtensa OCD Daemon v14.08

Xtensa Xplorer v9.0.18

 

<Compiled DSP bin Size>

    dsp_data_debug.bin: 1153KB

    dsp_ncache_debug.bin: 11KB

    dsp_text_debug.bin: 130KB

 

<Error Message: below image>

xtensa_error.PNG

 

please let me know if more information is needed or how can I fixed this error. 

 

Best Regards

gnani

0 Kudos
15 Replies

2,092 Views
jason_tseng
NXP Employee
NXP Employee

Hello Gnani,

XOCD log shows the access to memory location 0x428a0038 failed with a data error resulting in exception to get triggered.

system memory map is included in linker support packages, pls ref to elf32xtensa.x under ldscripts folder

Let's focus on xt-ocd error on this ticket.

If you still have question about memory configuration, pls create another ticket for tracking.

Thanks

Best Regards
Jason Tseng

0 Kudos

2,088 Views
gnani
Contributor I

Hello Jason Tseng,

Thank you for your reply.

Have a nice day!

 

Best Regards

Gnani

0 Kudos

2,111 Views
jason_tseng
NXP Employee
NXP Employee

Hello Gnani,

Thanks for the confirmation.

That makes more sense to me.

 

Do you have source code of customized voip library?

Please try to review the code and see where to cause the error.

Obviously there are some piece of codes in voip lib access invalid address.

Thanks

Best Regards

Jason Tseng

0 Kudos

2,099 Views
gnani
Contributor I

Hello Jason,

I have one more question.

I am debugging "Changing the Memory Map" refer to Xtensa Linker Support Packages(LSPs) Reference Manual (lsp_rm.pdf) document.

I want to expand dram/iram size using "xt-genldscripts"

 

Please refer to attached memmap.xmm file.

 

Below is an image when ldscripts are created normally.

111.PNG

 

Test 1

Modify dram size from 0x10000 to 0x20000 in memmap.xmm file.

Below is an error image

222.PNG

Test 2

Modify iram size from 0x10000 to 0x20000 in memmap.xmm file.

Below is an error image 333.PNG

 

Question)

Is it possible to change the size of iram and dram?

Please let me know If possibe.

 

Thank you for your help.

Best Regards

Gnani

0 Kudos

2,106 Views
gnani
Contributor I

Hello Jason,

Thank you for your reply.

Unfortunately I don't have source code of customized voip library.

So I request to my customer to review the code and see where to cause the error.

 

By the way.. I want to know some more.

1. What is the exact meaning of below log.

  (Refer to Memory Configuration, I'm just able to know "epcdbg:2402063c" means iram0_8_seg origin)

==========================================================================

Error: Exception details: exccause:0xd, excvaddr:0x428a0038, epc:0x1cfe24, epcdbg:2402063c
Error: Op 'xtensa_read_memory' failed, will not retry

==========================================================================

- Memory Configuration
Name                        Origin             Length            Used               Unused
dsp_core_seg           0x00200000   0x00280000   0x0010ee58    0x001711a8
dsp_uncached_seg  0x20060000   0x00010000    0x00002990    0x0000d670
dram0_0_seg           0x24000000   0x00010000    0x0000000c    0x0000fff4
iram0_0_seg            0x24020000   0x00000400    0x0000014c    0x000002b4
iram0_1_seg            0x24020400   0x0000017c    0x0000016c    0x00000010
iram0_2_seg            0x2402057c   0x00000020    0x0000001c    0x00000004
iram0_3_seg            0x2402059c   0x00000020    0x0000000c    0x00000014
iram0_4_seg            0x240205bc   0x00000020    0x0000000c    0x00000014
iram0_5_seg            0x240205dc   0x00000020    0x0000000c    0x00000014
iram0_6_seg            0x240205fc    0x00000020    0x0000000c    0x00000014
iram0_7_seg            0x2402061c   0x00000020    0x00000018    0x00000008
iram0_8_seg            0x2402063c   0x0000f9c4     0x00000008    0x0000f9bc
*default*                   0x00000000   0xffffffff

==========================================================================

2. If voip process() use more memory (maybe customer use malloc, memset, memcpy and etc.. ), shouldn't I expand the IRAM or DRAM(exactly I don't know) area? Please let me know if you know how to adjust RAM area?

 

Thanks

Best Regards

Gnani

0 Kudos

2,116 Views
jason_tseng
NXP Employee
NXP Employee

Hello Gnani,

After step  3) Run "xt-ocd -c topology.xml" on window command

There is no error and log msg shows "Warning: Warning: DAP Reset request failed! Ignoring." 

Then log message stop here.

But after step 5) Typed "record_dmic" and step 6) Result             if there is voip process()

Then log message will continuous to show "Warning: Target not under control. No status update performed"

and other other error message.

 

Is above understanding correct?

 

Thank

Best Regards
Jason Tseng

 

0 Kudos

2,114 Views
gnani
Contributor I

Hello Jason,

After step 3) Run "xt-ocd -c topology.xml" on window command
There is no error and log msg shows "Warning: Warning: DAP Reset request failed! Ignoring."
Then log message stop here.

xt-ocd_1.PNG

But after step 5) Typed "record_dmic" and step 6) Result: if there is voip process()
Then log message will continuous to show "Warning: Target not under control. No status update performed"
and other other error message.

 -> Yes that's right.

 -> After run "record_dmic" on serial window, displayed like below

xt-ocd_2.PNG

xt-ocd_3.PNG

You understand correctly.

 

Thank you for your help

Best Regards

Gnani

0 Kudos

2,119 Views
jason_tseng
NXP Employee
NXP Employee

Hello Gnani,

 

"But modified memmap.xmm file is no effect on motion."

What does that mean "no motion"?

 

" I can run jlink and xt-ocd on default sram settings and modification sram settings.

 But maybe added customized code(voip process part) will occur this error."

Do you mean after modified sram settings, jlink and xt-ocd are still working well???

But after customized voip lib added then you will see the error when run xt-ocd???

 

Please note: While making the debug connection the tools doesn't refer to the memmap files you modified. 

 

Thanks

Best Regards
Jason Tseng

0 Kudos

2,118 Views
gnani
Contributor I

Hello Jason,

I reply to your asking. Please refet to below

"But modified memmap.xmm file is no effect on motion."

What does that mean "no motion"?

(Please note: While making the debug connection the tools doesn't refer to the memmap files you modified.)

  -> No motion means No effect on board operation. I understood referring to your note.

Do you mean after modified sram settings, jlink and xt-ocd are still working well???

  -> Yes, That's right if modified sram settings I did was right. 

But after customized voip lib added then you will see the error when run xt-ocd???

  -> Yes that's right. Error occured step is like below

     1) Add customized voip lib and some code to xa_hw_capturer_read_FIFO() of xa_capturer-dmic.c

     2) Build dsp_xaf_record_hifi4 example

     3) Run "xt-ocd -c topology.xml" on window command

     4) Debug on Xtensa Xplorer & Run to AUD-EVK board on Xtensa Xplorer

     5) Typed "record_dmic" script on serial command window and run

     6) Result

        - Error msg occured on xt-ocd window command

             if there is voip process() on xa_hw_capturer_read_FIFO() of xa_capturer-dmic.c 

        - Error msg is not occured on xt-ocd window command

             if there is no voip process() on xa_hw_capturer_read_FIFO() of xa_capturer-dmic.c

     7) note: voip process() means customized voice filtering processing function

 

Thank you for your help.

Best Regards

Gnani

 

0 Kudos

2,124 Views
jason_tseng
NXP Employee
NXP Employee

Hello Gnani,

Except elf32xtensa.x, memmap.xmm and topology.xml, there is no other modifications, is that correct?

If you revert these modifications the error will not be shown, is that correct?

i.e using default settings you can run jlink and xt-ocd without any issue, is that correct?

BTW, what sdk version you are using?

ps: "SDK: dsp_xaf_record_hifi4" this is sdk example you are using, but I would like to know exact sdk version.

Thanks

Best Regards
Jason Tseng

0 Kudos

2,121 Views
gnani
Contributor I

Hello Jason,

I reply to your asking. Please refer to below.

 

Except elf32xtensa.x, memmap.xmm and topology.xml, there is no other modifications, is that correct?

  -> Yes, that's right. But modified memmap.xmm file is no effect on motion.

 

If you revert these modifications the error will not be shown, is that correct?

i.e using default settings you can run jlink and xt-ocd without any issue, is that correct?

  -> I can run jlink and xt-ocd on default sram settings and modification sram settings.

      But maybe added customized code(voip process part) will occur this error.

      So I tested sram size modification test.

      If these error messages means DRAM error, please let me know how to modify DRAM area.

 

BTW, what sdk version you are using?

ps: "SDK: dsp_xaf_record_hifi4" this is sdk example you are using, but I would like to know exact sdk version.

  -> Release Version: 2.11.1 (SDK_2_11_1_MIMXRT685-AUD-EVK)

  ->  I am using dsp_xaf_record_hifi4" this is sdk example.

 

Thank you for your help

Best Regards

Gnani

 

0 Kudos

2,137 Views
jason_tseng
NXP Employee
NXP Employee

Hello Gnani,

Do you use Linker support package?

If yes, please also provide it from devices\MIMXRT685S\xtensa\gdbio for reference.

 

Meanwhile, what modifications you made for memory address?

Please also list the details about your changes and updates related files.

Thanks

Best Regards
Jason Tseng

0 Kudos

2,135 Views
gnani
Contributor I

Hello Jason,

Yes, I use Linker support package.

I attached gdbio zip file.

 

<Modification>

1. Add Customized voip Library (about 920KB) in gdbio folder

(Customized voip library is my customer's. Please let me know if you need this library.)

2. Modify some part of xa-capturer-dmic.c 

3. Set XA_VIT_PRE_PROC to 0

 

<Debugging History>

I think SRAM size of DSP(HiFi4) is not  enough capacity.

So I just modify SRAM size of CM33 from 1.5MB to 0.5MB on MCUXplorer IDE.

        Memory region         Used Size  Region Size  %age Used
                    SRAM:          116780 B       512 KB        22.27%

And I modify elf32xtensa.x file for expand sram size from 2.5MB to 3.5MB (refet to attached zip file)

    dsp_xaf_record_hifi4.map

        Name                  Origin                Length                Used               Unused          Attributes
    dsp_core_seg     0x00100000      0x00380000      0x00129c08      0x002563f8

I can not modify RAM size modification because I don't know how to change DRAM/IRAM size. 

 

Thank you for your help.

Please let me know if you have any questions.

 

Best Regards
Gnani

 

0 Kudos

2,162 Views
jason_tseng
NXP Employee
NXP Employee

Hello Gnani,

Could you provide your  config.html and topology.xml for our reference?

Thanks

Best Regards
Jason Tseng

0 Kudos

2,142 Views
gnani
Contributor I

Hello Jason,

I attached two files(config.html and topology.xml) in zip file

topology.xml is in C:\Program Files (x86)\Tensilica\Xtensa OCD Daemon 14.08,

config.html is in SDK_2_11_1_MIMXRT685-AUD-EVK\middleware\fatfs\documents\doc path.

Please let me know if it's not the file you want.

Thanks

 

Best Regards

Gnani

0 Kudos