MIMXRT595 I3C interface not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT595 I3C interface not working

840 Views
gilmotta2
Contributor II

This is kind of urgent if you could assist me I would appreciate it. We told our customers to buy the same EVK boards but it does not work now our project is on HOLD pending this issue.

I purchased two MIMXRT595-EVK boards, I have them inter-connected via the I3C connector at location J18 on the board.

 

rt595_I3C_connector_J18.PNG

 

I have the SDK Master demo running on one board and the SDK Slave demo running on the other board and I don’t see any traffic from I2C or I3C.

Slave

slave_output.png

Master

master_output.png

 

0 Kudos
1 Reply

831 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @gilmotta2 ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I was wondering if you can tell me which version of the SDK library you used, further, I'd like to suggest you use the logic analyzer to visualize the transmit signals.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos