Hi All
I am trying to create a basic project in MCUExpresso IDE for the MIMXRT106S processor using the Project Create Wizard.
After the project is created, I try to build it and it fails with 7 errors.
Are there any special settings for this processor?
Hi @seandutoit ,
You can use Security Provisioning tool to connect RT106s via serial mode. Let it recognize the flash, make a full erase.
Then you need a flash download algorithm for IDE downloading and FCB for flexspi config. Different flash may has different algorithm and FCB.
Regards,
Jing
As this chip is a brand new chip from the factory, Is there anything special I should do before trying to program it. I am even trying to run a application from RAM but that also is not working.
Is there a minimum number of pins that should be connected before programming the device. Maybe I am missing a pin connection. Where should the JTAG_nRST from debugger be connected? I now have it on Pin G10.
I have Boot Mode0 and Boot Mode1 pins connected. Are any of the other pins important on a new device?