I tried downloading pre-built HelloWorld example to get familiar with the board. After build, when I try to connect to via debugging, IDE shows me the "0 available SWD Devices detected" error.
Help me resolve this!
Regards,
Zeke
I fixed it and I am able to access the board via debugger now.
Regards,
Zeke
Hello,
How did you solve it? I'm having the same problem.
Thanks!
You need to modify SW7 switch configuration in NXP board
Mark this solution as Helpful and Correct if it works for you
Regards,
Zeke
Hi, Zeke.
The SW7 was already 0001 when I got the no device detected error.
When you say download program, you mean the program I want to debug to be downloaded with the debugger, right?
Well, that's when I get the error, so I never get a successful download...
Best regards,
Haddad
Hi Marco,
I never faced this issue when SW7 position was 0001. As I never faced this before, I do not have a solution readily available.
Regards,
Zeke