MIMXRT1060-EVK, Design files for Altium Designer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1060-EVK, Design files for Altium Designer

1,405 Views
mykes
Contributor I

Would it be possible to get an ascii export of the .brd file. This would be an extension .alg.  Altium can then import this, but this file can only be created from a Allegro licensed PC.

Regards

Geir Myklatun

Labels (1)
0 Kudos
9 Replies

1,198 Views
chads108
Contributor I

Would also be possible to get an ascii export of LAY-31399_C.brd from the  8M MINI EVK LPDDR4 CM_Rev C Customer Release Package?

0 Kudos

1,198 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello Chad,

Unfortunately, I have not the information for 8M MINI EVK lPDDR4. Sorry for the inconvenience may cause.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

1,198 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

I provide the reference file via email. Hope it help you.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

1,198 Views
mykes
Contributor I

Hello fangfang,

I am still waiting for the ascii export of the .brd file.

Regards

Geir

0 Kudos

1,198 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

I sent it to your email . Please check it again. Thanks

0 Kudos

1,198 Views
mykes
Contributor I

Hello,

Sorry, but I can’t find I have received an e-mail from you with the design file attached. Can you please try to send it once again?

Regards

Geir

Fra: fangfang <admin@community.nxp.com>

Sendt: tirsdag 23. april 2019 04.17

Til: Geir Myklatun <geir.myklatun@mykes.no>

Emne: Re: - Re: MIMXRT1060-EVK, Design files for Altium Designer

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community

Re: MIMXRT1060-EVK, Design files for Altium Designer

reply from fangfang <https://community.nxp.com/people/fangfang?et=watches.email.thread> in i.MX RT - View the full discussion <https://community.nxp.com/message/1142340?commentID=1142340&et=watches.email.thread#comment-1142340>

0 Kudos

1,198 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

I just sent the reference files again. Please check it.

0 Kudos

1,116 Views
avbot
Contributor III

Hi, we urgently require these files also - please can you send to us?
Thanks!!!

0 Kudos

1,198 Views
mykes
Contributor I

Hi fangfang,

Thanks a lot.  I'm still waiting for the reference file, but will inform you as soon as I have received it and tried it with the importer.

Regards

Geir

0 Kudos