MIMXRT1060-EVK: Bootloader Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1060-EVK: Bootloader Mode

Jump to solution
2,621 Views
matthiasroedder
Contributor III

Hello Everyone,

I'm using the MIMXRT 1060 Evaluation Kit and I'm trying to start the Board in Bootloader Mode. I know this might seem stupid to ask but: How can I do this? 

I tried  keeping reset button pressed, while connecting the USB cable to the SDA USB port, but this does not work.

Happy Holidays!

Thank you in advance. 

Best regards, Matthias.

0 Kudos
1 Solution
2,616 Views
mjbcswitzerland
Specialist V

Hi

See page 14 of https://www.utasker.com/docs/iMX/uTaskerV1.4_iMX.pdf
i.MX RT 10160 board has its dip swithes on the top of the board though.

Regards

Mark

 

View solution in original post

7 Replies
2,608 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I've attached a document that demonstrates how to force the i.MX RT1060 enter the Serial Downloader mode, please refer to it for details.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,565 Views
matthiasroedder
Contributor III

Hey,

thank you for your Reply. Where can I find the attached document? Sorry I'm new here

Happy New Year!

Matthias

0 Kudos
2,617 Views
mjbcswitzerland
Specialist V

Hi

See page 14 of https://www.utasker.com/docs/iMX/uTaskerV1.4_iMX.pdf
i.MX RT 10160 board has its dip swithes on the top of the board though.

Regards

Mark

 

2,555 Views
matthiasroedder
Contributor III

Hi,

thank you for the tips! I have tried this, but I always have the same error "Cannot find USB-HID device (vid=0x1FC9, pid=0x0135, please connect USB cable to your board first!"

The board ist connected to my PC and the Boot Mode Switches configurated as described in the document. 

Happy New Year!

Matthias

0 Kudos
2,547 Views
mjbcswitzerland
Specialist V

Hi

Have you connected the USB cable?

It is not the one that is used to power the board. You also need to connect a second one to the processor's USB device socket.

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or rapid product development requirements

For professionals searching for faster, problem-free Kinetis and i.MX RT 10xx developments the uTasker project holds the key: https://www.utasker.com/iMX/RT1060.html

2,529 Views
matthiasroedder
Contributor III

Hi

I have connected the USB cable to the Debug USB on the Board. Do I have to use the "USB Host" or the "USB OTG" additionally? 

I attached a picture of the Board to make clear what I mean.

Thank You!

Matthias 

mimxrt1060-evk.jpg

0 Kudos
2,524 Views
matthiasroedder
Contributor III

Okay yeah I have to connect the Debug USB and the USB OTG to my PC and then it works! 

Thank you @mjbcswitzerland !  

Regards

Matthias

0 Kudos