MIMXRT1050EVK ‘sd_jpeg' example free run error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MIMXRT1050EVK ‘sd_jpeg' example free run error

971 次查看
ray_deng
Contributor II

Dears,

  I got stuck at MIMXRT1050EVK ‘sd_jpeg' example free run, it report '-4' error. While debug OK.

  Can you help to advice?

BRs,

Ray

标签 (1)
0 项奖励
4 回复数

875 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I think I need more information about the issue, so I was wondering if you can introduce what modification you do about the sd_jpeg demo.
In addition, the testing process and IDE, etc

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励

875 次查看
ray_deng
Contributor II

Hi Jeremy,

  Thanks for your response.

  I just modified the picture size to 800x480 pixel with picture number 76 from 000.jpeg to 075.jpeg. Built in Keil MDK Ver. 5.29 for target sd_jpeg_flexspi_nor_sdram_debug. It debugs OK, but free run error, report error "-4".

BRs,

Ray

0 项奖励

875 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thanks for your reply.
For caution's sake, I wish you can present the exact modifications you did.

Looking forward to your reply.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励

875 次查看
ray_deng
Contributor II

Hi Jeremy,

  

    I fixed, it is caused by TF Card,

BRs,

Ray