MCU-Link Debug Probe Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU-Link Debug Probe Issue

1,923 Views
BTasdemir
Contributor I

We are using imx rt1176 evk. Onboard debugger are working. But we have to use MCU-Link Debug Probe. Debugger Link 

When I try to debugging with the MCU Link debug probe, I get an error like
in the pictures.

BTasdemir_0-1695134657493.pngBTasdemir_1-1695134710740.png

How can i solve this problem ?

0 Kudos
Reply
7 Replies

1,860 Views
BTasdemir
Contributor I

Im using RT1170 EVK and SWD interface. I removed J6 J7 but still same error. 

 

RT1170EVK.jpg

0 Kudos
Reply

1,773 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I suggest use an adapter to use the JTAG port as a SWD flavor. I made a document related to this issue; I hope this explain more.

Best regards,
Pavel

 

0 Kudos
Reply

1,858 Views
Masmiseim
Senior Contributor I

Hello @BTasdemir 

you are using the wrong JTAG interface. This one is to debug the onboard Freelink Interface (the LPC4322 controller)

You need to use the 20-Pin JTAG interface.

Regards

0 Kudos
Reply

1,851 Views
BTasdemir
Contributor I
Hello,
Thanks for reply
How can i use 20 pin jtag with this cable ? am i need converter ?
0 Kudos
Reply

1,847 Views
Masmiseim
Senior Contributor I
0 Kudos
Reply

1,870 Views
lucas_cao
NXP Employee
NXP Employee

If you are using RT1170 EVK, please remove J6 and J7.

if you are using RT1170 EVKB, please add a jumper on JP5.

0 Kudos
Reply

1,885 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I do not if you are using your MCU Link in the right interface, could you please elaborate further about the connector you are using for communicating the external debugger? please review the document.

Best regards,
Pavel

0 Kudos
Reply