I have found the TCR[BYSW] bit in LPSPI useful for transmitting large byte oriented object files using LPSPI. To use this bit, I need to modify the SDK as the SDK does not modify this bit in LPSPI_Init.
It's pretty simple to add a byteSwap field to the config struct, would you be able to add this functionality to a future SDK release?
解決済! 解決策の投稿を見る。
Hi @gavin5342,
You are correct, the usage of the Byte Swap bit on the Transmit Command (TCR) is not fully implemented on our LPSPI drivers. I will comment this to the SDK team so they can take a look at it and make the proper adjustments if they consider them appropriate (which, as you mention, shouldn't require much work at all).
Thanks for reporting this!
BR,
Edwin.
Hi @gavin5342,
You are correct, the usage of the Byte Swap bit on the Transmit Command (TCR) is not fully implemented on our LPSPI drivers. I will comment this to the SDK team so they can take a look at it and make the proper adjustments if they consider them appropriate (which, as you mention, shouldn't require much work at all).
Thanks for reporting this!
BR,
Edwin.