Is there a reference document for the i.MX RT1064 internal ROM API?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a reference document for the i.MX RT1064 internal ROM API?

1,329 Views
jcforlc
Contributor I

Specifically looking for information on programming the 4MB QSPI Internal Flash using the ROM API routines described in the RT1064 reference manual.

Labels (1)
0 Kudos
2 Replies

968 Views
Yuri
NXP Employee
NXP Employee

Hello,

 Customers can refer to app note AN12263 (HABv4 RVT Guidelines and Recommendations)

https://www.nxp.com/docs/en/application-note/AN12263.pdf 

Regards,

Yuri.

0 Kudos

968 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi John Coppola,

    About the ROM API usage, you can refer to the RT1064 reference manual, there has a FLASH API examples on the RT1064-EVE board.

https://www.nxp.com/docs/en/reference-manual/IMXRT1064RM.pdf 

Page 268

pastedImage_2.png

Wish it helps you!

If you still have question about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos