For our target PCB, we need the GPIO that are used for Boot Configuration.
We would like to set the eFuses for BOOT_CFG1 and BOOT_CFG2 to set up QSPI NOR Flash.
To make the eFuses take effect, we have to set BT_FUSE_SEL=1.
But then, can we still access Serial Download?
The Reference Manual (table 21-9, page 1114) does not specify what happens if BT_FUSE_SEL==1 and boot_mode=01 (Serial Download).
Thanks,
Chris.
解決済! 解決策の投稿を見る。
Hi Chris Cowdery ,
Even you configure BT_FUSE_SEL=1, when you configure the BOOT_MODE[1:0]=01b, you still can enter the serial downloader mode, it is no relationship with BT_FUSE_SEL, just when you configure BOOT_MODE[1:0]=00b, then the ROM bootloader will check BT_FUSE_SEL.
So, don't worry, if your board still has the BOOT_MODE two pins avaiable, you still can enter the serial download mode.
Wish it helps you!
If you still have questions about it, please kindly let me know.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
---------------------------------------------------------------------------
Hi Chris Cowdery ,
Even you configure BT_FUSE_SEL=1, when you configure the BOOT_MODE[1:0]=01b, you still can enter the serial downloader mode, it is no relationship with BT_FUSE_SEL, just when you configure BOOT_MODE[1:0]=00b, then the ROM bootloader will check BT_FUSE_SEL.
So, don't worry, if your board still has the BOOT_MODE two pins avaiable, you still can enter the serial download mode.
Wish it helps you!
If you still have questions about it, please kindly let me know.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
---------------------------------------------------------------------------
Thankyou Kerry.