Interface with AD9364

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interface with AD9364

786件の閲覧回数
Anburaja
Contributor I

Hi,

I want to configure and control the AD9364 with i.MX RT1170 controller ,if it is possible?

0 件の賞賛
返信
5 返答(返信)

778件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Anburaja ,

   In fact, whether the AD9364 is supported, just check your used chip interface, I check it, find it contains the SPI, and parallel interface.

  So, RT1170 can support it, as it contains the LPSPI and the flexIO support the parrallel, even the normal GPIO also can use as the parallel input and output.

Best Regards,

kerry

 

0 件の賞賛
返信

773件の閲覧回数
Anburaja
Contributor I

Thanks for your reply Kerry,

You suggested [RT1170], it works up to 1 GHz, but I need to use up to 3 GHz, any other IC?

0 件の賞賛
返信

763件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Anburaja ,

  To the MCU, no 3GHz, the highest is 1Ghz.

   If you need higher speed, you may need to check the MPU, not the MCU.

 BTW, do you mean your chip spi and the parallel IO is up to 3Ghz, I don't think that is possible.

   Maybe you need to double check your requirement at first.

 

Best Regards,

Kerry

0 件の賞賛
返信

743件の閲覧回数
Anburaja
Contributor I

ok fine.

Is there any other way to make the MCU or MPU work up to 3GHz? Send if suitable IC available.

 

Thanking you..!

0 件の賞賛
返信

738件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Anburaja ,

  At least our RT have no way to run upto 3G, as you know, the core is just upto 1G.

  To the MPU, you may check it in this area, you can create a new question about MPU :

https://community.nxp.com/t5/i-MX-Processors/bd-p/imx-processors

Not the RT, then our MPU engineer will help you.

 

Wish it helps you!

Best Regards,

kerry

0 件の賞賛
返信