IP Write to HyperRam on IMXRT1064

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IP Write to HyperRam on IMXRT1064

1,715件の閲覧回数
etc
Contributor I

When using the ipwrite command to send data to HyperRam we find a multiple microsecond delay between the DUMMY_RWDS_DDR command and the WRITE_DDR command.  The delay only happens between CA and the first burst of data.  Is there an explanation for that delay?  Or some way to shorten it?

0 件の賞賛
2 返答(返信)

1,694件の閲覧回数
jay_heng
NXP Employee
NXP Employee

Do you see the same issue when using AHB write?

0 件の賞賛

1,640件の閲覧回数
etc
Contributor I

I do not.  There is no delay between the DUMMY_RWDS command and the WRITE_DDR command in an AHB write. 

 

I do see a 15us delay between ahb write bursts that I assume is either the AHB_TX_BUF or the TX_FIFO  reloading.  It is difficult to ascertain what is going on between those two data sources.

0 件の賞賛