IMXRT1176 ENETQOS USING KSZ 8081 PHY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT1176 ENETQOS USING KSZ 8081 PHY

497件の閲覧回数
wangdabing
Contributor I

hello supporter, In My Customized imrt1176 board ,we use the ENET_QOS MAC  to connect a KSZ8081 PHY, with "enet_qos_txrx_mulitring sdk example " ,we can get the phy id from the mdio interface ,we can 

auto negoiate from the remote 100M port ,but we failed at DMA reset ,following is the Schematic , please help to review it .

wangdabing_0-1651042492511.png

 

0 件の賞賛
1 返信

490件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello @wangdabing .

From the schematic and I can't find the obvious issue and you may check the config of the development board as the below:

fangfang_0-1651198466727.png

 

 

Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛