IMXRT1170-EVK how-to configure multicore project use of BOARD_SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1170-EVK how-to configure multicore project use of BOARD_SDRAM

Jump to solution
162 Views
galenhevo
Contributor II

I am finding most of the single core cm7 projects are loading code into BOARD_SDRAM (which is large)

galenhevo_0-1714573710116.png

in multicore projects no BOARD_SDRAM is initialized and code is loaded into SRAM_DTC_cm7, though the required shared memory is initialized:

galenhevo_1-1714573827238.png

What would be the best way to combine these two memory layouts so that I might utilize the much larger BOARD_SDRAM for my code while still retaining shared memory layout between the CM7/CM4? What files need to be updated/configurations in MCUXpresso IDE, as I'm seeing most of the link/map files are auto-generated?

 

0 Kudos
1 Solution
93 Views
galenhevo
Contributor II

Thanks for the response Omar.  That's not exactly what I was asking.  I tried a few different memory layouts and was able to find one that was acceptable and worked after setting the XIP_BOOT_HEADER_DCD_ENABLE=1.  Without that the system would hardfault and I would have to recover using the MCU Boot Utility. 

I found some explanation of the flag in this application note: https://www.nxp.com/docs/en/nxp/application-notes/AN12183.pdf

View solution in original post

0 Kudos
2 Replies
94 Views
galenhevo
Contributor II

Thanks for the response Omar.  That's not exactly what I was asking.  I tried a few different memory layouts and was able to find one that was acceptable and worked after setting the XIP_BOOT_HEADER_DCD_ENABLE=1.  Without that the system would hardfault and I would have to recover using the MCU Boot Utility. 

I found some explanation of the flag in this application note: https://www.nxp.com/docs/en/nxp/application-notes/AN12183.pdf

0 Kudos
113 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

You can use SDRAM to load code so CM4 fetch from there: How to move CM4 core project to SDRAM in RT1176 - NXP Community

Most of the examples use TCM as it has the best performance as it is nearer to the core.

Best regards,
Omar