IMXRT1024 LPUART Transmit Output and TXD Pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1024 LPUART Transmit Output and TXD Pin

Jump to solution
907 Views
Lukas_Frank
Senior Contributor I

Hi all,

 

Q.1. What is the difference between transmitter output and TXD Pin? Isn't already the output of the transmitter TXD Pin? Where is the transmitter output in figure 44-1?

Lukas_Frank_1-1625656871384.png

Q.2. Whhy we use TXINV and RXINV? Why we need to inverse/reverse polarity of transmitted data output?

 

Thanks and Regards.

 

0 Kudos
Reply
1 Solution
895 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Q.1. What is the difference between transmitter output and TXD Pin? Isn't already the output of the transmitter TXD Pin? Where is the transmitter output in figure 44-1?

Transmitter output and TXD pin are the same things. 

Q.2. Whhy we use TXINV and RXINV? Why we need to inverse/reverse polarity of transmitted data output?

You don't need to invert these signals, however, the module gives you the option to do so in case your working environment demands it. This is mentioned in the LPUART Control Register and LPUART Status Register. 

Regards,
Victor

View solution in original post

0 Kudos
Reply
1 Reply
896 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Q.1. What is the difference between transmitter output and TXD Pin? Isn't already the output of the transmitter TXD Pin? Where is the transmitter output in figure 44-1?

Transmitter output and TXD pin are the same things. 

Q.2. Whhy we use TXINV and RXINV? Why we need to inverse/reverse polarity of transmitted data output?

You don't need to invert these signals, however, the module gives you the option to do so in case your working environment demands it. This is mentioned in the LPUART Control Register and LPUART Status Register. 

Regards,
Victor

0 Kudos
Reply