IMXRT1020 PMIC_ON_REQ without separate DCDC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1020 PMIC_ON_REQ without separate DCDC

779 Views
kirstein
Contributor I

I am using a single 3.3V for Driving the IMXRT1020 power pins, because I do not need the power saving modes.

So I do not need power sequencing and there is no need to turn on an external DCDC.

How to connect "PMIC_ON_REQ" in this case ?

Labels (1)
1 Reply

710 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Martin,

 

If the pin is not used it can be left floating.

 

Regards,

Felipe