IMX.RT1064 can not wakeup by magic packet (WOL)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX.RT1064 can not wakeup by magic packet (WOL)

793 Views
zrx
Contributor II

Hello NXP team,

i want to use magic packet to wakeup my rt1064board, then i follow the IMXRT1064RM.pdf

1. set the ECR[MAGICEN] and ECR[SLEEP] BIT,  the mac enter the sleep mode.

2.Then i use udp send a magic packet to the imxrt1064 board. Before first step,the board can recieve the magic packet,but after the first step the EIR[WAKUP] can not set.

Here is the code,

 

int macsleep111(void)
{
 // ENET_EnableSleepMode(ENET,1);
  ENET->ECR |= (1 <<2 );
  ENET->ECR |= (1 <<3 );

  DisableIRQ(ENET_IRQn);
  ENET_EnableInterrupts(ENET,ENET_ERR_INTERRUPT|kENET_WakeupInterrupt );
  NVIC_ClearPendingIRQ(ENET_IRQn);
  NVIC_EnableIRQ(ENET_IRQn);
  EnableIRQ(ENET_IRQn);
  LPM_EnableWakeupSource(ENET_IRQn); 
  return 0;
}
MSH_CMD_EXPORT(macsleep111, wakeup_demo );

 

magic detection.PNGmagicpacket.PNGrecieve frame.PNG

 

 

 

 

Labels (1)
Tags (2)
0 Kudos
3 Replies

747 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @zrx,

I did try also this feature without success. I will investigate this issue and let you know as soon as I made some progress.

Best Regards,

Alexis Andalon

0 Kudos

724 Views
zrx
Contributor II

here you should add the kENET_WakeupInterrupt interrupt

#define ENET_ERR_INTERRUPT \
(kENET_BabrInterrupt | kENET_BabtInterrupt | kENET_EBusERInterrupt | kENET_LateCollisionInterrupt | \
kENET_RetryLimitInterrupt | kENET_UnderrunInterrupt | kENET_PayloadRxInterrupt |kENET_WakeupInterrupt)

so enet can set error handler when init the enet intterupt
here is the code:

static void ENET_SetHandler(ENET_Type *base,
enet_handle_t *handle,
const enet_config_t *config,
const enet_buffer_config_t *bufferConfig)
{
uint8_t count;
uint32_t instance = ENET_GetInstance(base);
const enet_buffer_config_t *buffCfg = bufferConfig;

/* Store transfer parameters in handle pointer. */
memset(handle, 0, sizeof(enet_handle_t));

handle->ringNum = (config->ringNum > FSL_FEATURE_ENET_QUEUE) ? FSL_FEATURE_ENET_QUEUE : config->ringNum;
for (count = 0; count < handle->ringNum; count++)
{
assert(buffCfg->rxBuffSizeAlign * buffCfg->rxBdNumber > config->rxMaxFrameLen);

handle->rxBdBase[count] = buffCfg->rxBdStartAddrAlign;
handle->rxBdCurrent[count] = buffCfg->rxBdStartAddrAlign;
handle->rxBuffSizeAlign[count] = buffCfg->rxBuffSizeAlign;
handle->txBdBase[count] = buffCfg->txBdStartAddrAlign;
handle->txBdCurrent[count] = buffCfg->txBdStartAddrAlign;
handle->txBuffSizeAlign[count] = buffCfg->txBuffSizeAlign;
buffCfg++;
}

/* Save the handle pointer in the global variables. */
s_ENETHandle[instance] = handle;

/* Set the IRQ handler when the interrupt is enabled. */
if (config->interrupt & ENET_TX_INTERRUPT)
{
s_enetTxIsr = ENET_TransmitIRQHandler;
EnableIRQ(s_enetTxIrqId[instance]);
}
if (config->interrupt & ENET_RX_INTERRUPT)
{
s_enetRxIsr = ENET_ReceiveIRQHandler;
EnableIRQ(s_enetRxIrqId[instance]);
}
if (config->interrupt & ENET_ERR_INTERRUPT)
{
s_enetErrIsr = ENET_ErrorIRQHandler;
EnableIRQ(s_enetErrIrqId[instance]);
}
}


then the EIR[WAKEUP] can be set by magic packet,but can not wakeup by magic packet.
here is the code:
int enetwakeup(void)
{
uint32_t freq;
int i = 0;

/* When wakeup from suspend, peripheral's doze & stop requests won't be cleared, need to clear them manually */
IOMUXC_GPR->GPR4 = 0x00000000;
IOMUXC_GPR->GPR7 = 0x00000000;
IOMUXC_GPR->GPR8 = 0x00000000;
IOMUXC_GPR->GPR12 = 0x00000000;

CLOCK_SetMux(kCLOCK_UartMux, 1);
CLOCK_SetDiv(kCLOCK_UartDiv, 0);

BOARD_InitBootPeripherals();
DEBUG_MSG("\r\nCPU wakeup source 0x%x...\r\n", SRC->SRSR);
APP_PrintRunFrequency(0);

LPM_Init();
APP_PowerModeSwitch(s_curRunMode);
ENET_EnableSleepMode(ENET,1);
while (1)
{
freq = CLOCK_GetFreq(kCLOCK_CpuClk);
DEBUG_MSG("\r\n########## Power Mode Switch Demo %d times(build %s) ########### \n\r\n", i++,__DATE__);
DEBUG_MSG(" Core Clock = %dHz \r\n", freq);
APP_ShowPowerMode(s_curRunMode);

s_targetPowerMode = LPM_PowerModeSysIdle;
if (s_targetPowerMode <= LPM_PowerModeEnd)
{
/* If could not set the target power mode, loop continue. */
if (!APP_CheckPowerMode(s_curRunMode, s_targetPowerMode))
{
continue;
}

DisableIRQ(ENET_IRQn);
ENET_EnableSleepMode(ENET,1);

NVIC_ClearPendingIRQ(ENET_IRQn); //唤醒源的设置
ENET_EnableInterrupts(ENET,kENET_WakeupInterrupt ); //使能错误中断 唤醒中断
NVIC_EnableIRQ(ENET_IRQn);
EnableIRQ(ENET_IRQn);
LPM_EnableWakeupSource(ENET_IRQn); //使能唤醒源

ENET->ECR |= 0X02; //使能网卡

APP_PowerPreSwitchHook(s_targetPowerMode);
APP_PowerModeSwitch(s_targetPowerMode);
APP_PowerPostSwitchHook(s_targetPowerMode);

// ENET_EnableSleepMode(ENET,0);// MAC退出休眠
}
DEBUG_MSG("\r\nNext loop\r\n");
}
}

so please let me know when you make some progress. thank you.

 

0 Kudos

710 Views
zrx
Contributor II

 

about this enet intterupt ,you you should add kENET_WakeupInterrupt here

#define ENET_ERR_INTERRUPT \
(kENET_BabrInterrupt | kENET_BabtInterrupt | kENET_EBusERInterrupt | kENET_LateCollisionInterrupt | \
kENET_RetryLimitInterrupt | kENET_UnderrunInterrupt | kENET_PayloadRxInterrupt |kENET_WakeupInterrupt)

so when you config the kENET_WakeupInterrup interrupt ,the enet can set error hanlder here,

static void ENET_SetHandler(ENET_Type *base, enet_handle_t *handle, const enet_config_t *config,
const enet_buffer_config_t *bufferConfig)
{
    uint8_t count;
   uint32_t instance = ENET_GetInstance(base);
   const enet_buffer_config_t *buffCfg = bufferConfig; 

   /* Store transfer parameters in handle pointer. */ 
   memset(handle, 0, sizeof(enet_handle_t));

  handle->ringNum = (config->ringNum > FSL_FEATURE_ENET_QUEUE) ?         FSL_FEATURE_ENET_QUEUE : config->ringNum;
  for (count = 0; count < handle->ringNum; count++)
 {
   assert(buffCfg->rxBuffSizeAlign * buffCfg->rxBdNumber > config->rxMaxFrameLen);

   handle->rxBdBase[count] = buffCfg->rxBdStartAddrAlign;
   handle->rxBdCurrent[count] = buffCfg->rxBdStartAddrAlign;
   handle->rxBuffSizeAlign[count] = buffCfg->rxBuffSizeAlign;
   handle->txBdBase[count] = buffCfg->txBdStartAddrAlign;
   handle->txBdCurrent[count] = buffCfg->txBdStartAddrAlign;
   handle->txBuffSizeAlign[count] = buffCfg->txBuffSizeAlign;
  buffCfg++;
}

  /* Save the handle pointer in the global variables. */
  s_ENETHandle[instance] = handle;

  /* Set the IRQ handler when the interrupt is enabled. */
 if (config->interrupt & ENET_TX_INTERRUPT)
 {
   s_enetTxIsr = ENET_TransmitIRQHandler;
   EnableIRQ(s_enetTxIrqId[instance]);
}


 if (config->interrupt & ENET_RX_INTERRUPT)
 {
   s_enetRxIsr = ENET_ReceiveIRQHandler;
   EnableIRQ(s_enetRxIrqId[instance]);
 }
 if (config->interrupt & ENET_ERR_INTERRUPT)
 {
  s_enetErrIsr = ENET_ErrorIRQHandler;
  EnableIRQ(s_enetErrIrqId[instance]);
 }
}

then the EIR[WAKEUP] can set by magic packet, but i can not wakeup by it in my rt1064 board.

here is my code,

int enetwakeup(void)
{
uint32_t freq;
int i = 0;
/* When wakeup from suspend, peripheral's doze & stop requests won't be cleared, need to clear them manually */
IOMUXC_GPR->GPR4 = 0x00000000;
IOMUXC_GPR->GPR7 = 0x00000000;
IOMUXC_GPR->GPR8 = 0x00000000;
IOMUXC_GPR->GPR12 = 0x00000000;

CLOCK_SetMux(kCLOCK_UartMux, 1);
CLOCK_SetDiv(kCLOCK_UartDiv, 0);

BOARD_InitBootPeripherals();
DEBUG_MSG("\r\nCPU wakeup source 0x%x...\r\n", SRC->SRSR);
APP_PrintRunFrequency(0);

LPM_Init();
ENET_EnableSleepMode(ENET,1);
while (1)
{
freq = CLOCK_GetFreq(kCLOCK_CpuClk);
DEBUG_MSG("\r\n########## Power Mode Switch Demo %d times(build %s) ########### \n\r\n", i++,__DATE__);
DEBUG_MSG(" Core Clock = %dHz \r\n", freq);
APP_ShowPowerMode(s_curRunMode);

s_targetPowerMode = LPM_PowerModeSysIdle;
if (s_targetPowerMode <= LPM_PowerModeEnd)
{
/* If could not set the target power mode, loop continue. */
if (!APP_CheckPowerMode(s_curRunMode, s_targetPowerMode))
{
continue;
}

DisableIRQ(ENET_IRQn);
ENET_EnableSleepMode(ENET,1);

NVIC_ClearPendingIRQ(ENET_IRQn);
ENET_EnableInterrupts(ENET,kENET_WakeupInterrupt );
NVIC_EnableIRQ(ENET_IRQn);
EnableIRQ(ENET_IRQn);
LPM_EnableWakeupSource(ENET_IRQn);

ENET->ECR |= 0X02;

APP_PowerPreSwitchHook(s_targetPowerMode);
APP_PowerModeSwitch(s_targetPowerMode);
APP_PowerPostSwitchHook(s_targetPowerMode);

// ENET_EnableSleepMode(ENET,0);/
}
DEBUG_MSG("\r\nNext loop\r\n");
}
}
MSH_CMD_EXPORT(enetwakeup, wakeup_demo );


so please let me know as soon as you made some progress,thank you.

 

 

0 Kudos