If I do a SetMux for I2C1 SDA off of GPIO_SD_B1_05 the XPRESSO/JLINK debug locks up. If I use AD_B1_01, there is no problem. If I single step, it then seems to jump over instructions and loop back over itself, so the debugger seems to be corrupted at that point.
解決済! 解決策の投稿を見る。
See this thread for an explanation:
-Nick
See this thread for an explanation:
-Nick
I also tried just to add a SetPinMux for SD_B1_05 to the flexspi_nor test software that was working and it now fails also. Moving to AD_B1_01 seems to work fine for the SDA signal but I will have to juggle board wiring as I am short GPIOs if I cannot use that one for some reason. Setting SD_B1_05 to SDA or plain GPI use does not matter, it causes problems anyway. Is there something special about this pin??
iMxRT1061A