I.MXRT1064 USB HOST ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MXRT1064 USB HOST ERROR

869 Views
raviranjankumar
Contributor III

Hi,

I am working on i.mxrt1064 USB. I am trying to connect one CDC device to processor host. Device is getting attached and enumeration is also done. But sometimes in USB_HostEhciTransactionDone API it is leading to transfer failed.

I am not able to find the issue, Please help.

Thanks and Regards,

Ravi Ranjan Kumar.

0 Kudos
1 Reply

755 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Ravi Ranjan Kumar,

Are you using our evaluation board or your own? Are you using the drivers we provide within the SDK? Are you using an example from the SDK or your own project? 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos