How to to download and program an application image into the external flash device for rt1050?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to to download and program an application image into the external flash device for rt1050?

1,501 次查看
starmichael
Contributor I

Using MfgTool2.exe to download and program an application image into the external flash device,it can't find the device.MfgTool2.exe Show "No Device Connected".The log massage is :

DLL version: 2.7.0
Monday, November 20, 2017 12:37:38 Start new logging
ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[1]: new KBLHidDeviceClass
ModuleID[2] LevelID[10]: Device Manager thread is running
ModuleID[2] LevelID[1]: Can't set m_hStopEvent before it initialized or it already stop

ModuleID[2] LevelID[10]: DeviceManager::DevChangeWnd::OnDeviceChange() - DEVICE_ARRIVAL_EVT(\\?\USB#VID_1FC9&PID_0130#5&352e360&0&13#{a5dcbf10-6530-11d2-901f-00c04fb951ed})
ModuleID[2] LevelID[10]: DeviceManager::DevChangeWnd::OnDeviceChange() - end
ModuleID[2] LevelID[10]: DeviceManager::OnMsgDeviceEvent() - DEVICE_ARRIVAL_EVT(\\?\USB#VID_1FC9&PID_0130#5&352e360&0&13#{a5dcbf10-6530-11d2-901f-00c04fb951ed})
ModuleID[2] LevelID[10]: DeviceClass::FindDeviceByUsbPath--DeviceListType_Current, _devices.size: 0
ModuleID[2] LevelID[1]: DeviceClass::FindDeviceByUsbPath() - DeviceListType_New--index: 0
ModuleID[2] LevelID[1]: DeviceClass::FindDeviceByUsbPath() - DeviceListType_New--devPath: \\?\hid#vid_1fc9&pid_0130#6&198f0cc1&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
ModuleID[2] LevelID[10]: new MxHidDevice[075E8768]

标签 (1)
0 项奖励
1 回复

1,289 次查看
joanxie
NXP TechSupport
NXP TechSupport

what external flash do you  use? when you connect PC to board, can your PC recognize your board? install any driver?

0 项奖励