I would like to test the master boot serial mode on an RT685. I have the MIMXRT685-EVK.
In the end I would like to have two RT685, one with a flash connected which boots then the other one via serial boot. For now I just want to test the serial boot though.
I assume if I link the software to be executable from RAM the resulting image file should be bootable via serial boot. If not, what else needs to be done in order to get a suitable image?
From the user manual I take that there are commands that are needed for the serial boot. Namely get_property, set_property and write_memory.
Is there a tool that NXP provides to do a serial boot from a host PC or do I have to implement this myself? If there is no tool, where do I find the documentation about those commands? I was not able to find anything.
Thanks for any help on this!
Solved! Go to Solution.
Thanks Miguel,
the blhost tool works to test this.
As for my other question, linking the application to RAM is sufficient to get a suitable image for this test, I tested it with the blhost tool.
Hi @lorv
These commands are for the blhost tool, this user guide will provide you more information of how to use it.
Best Regards, Miguel.
Thanks Miguel,
the blhost tool works to test this.
As for my other question, linking the application to RAM is sufficient to get a suitable image for this test, I tested it with the blhost tool.