Hello
Is there a possibility to interact with imx using high level programming (say detect button click ( e.g volume up key) using python/java) do you provide some sort of api or packets that can be used?
If not how else could i detect this?
Hello,
Devices of i.MX series have enough resources to support OS (Linux, Android, Win IoT).
This allows to use high level languages, based on OS.
As for i.MX RT series, please look at the following:
https://community.nxp.com/docs/DOC-345789
Regards,
Yuri.
Thanks for reply!
Yes i have installed Linux on imx hovewer i would like to detect events ( button click ( e.g volume up key)) from gui program. I am planning to add some simple gui using pyqt5 and in that aplication i would like to detect that event
So for example i have GUI application running on imx and user clicks volume up button on imx board and then using code in pyqt5 application i would like to save that in log