How to config RT1170 EVK to use on chip RAM only?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to config RT1170 EVK to use on chip RAM only?

Jump to solution
1,317 Views
ping1
Contributor V

Dear all

I am using EVK1170 and test with lwip_dhcp_freertos_cm7 example. 

I noticed it use external RAM by default, and I would like to config the project use internal RAM only, as my target board won't have any external RAM. Please let me know the procedure for that.

I tried remove delete RAM and RAM2 only from the memory editor below? what else do I need to do please?

ping1_0-1707144065125.png

Thank you!

Ping

0 Kudos
1 Solution
1,222 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @ping1 ,

  ITCM for NonCacheable setting also works on my side, please check my test result and the attached demo which I have written for you:

kerryzhou_0-1707400663526.png

kerryzhou_1-1707400671215.png

This is my DHCP test result:

kerryzhou_2-1707400688423.png

 

You can test it on your MIMXRT1170-EVK board.

Wish it helps you!

BTW, 2024 Chinese Spring Festival: Feb 9th to Feb 18th in total 10 days.
We will in the Spring Festival vacation, and back to work from 2.19th. During this time, you also can create the case, then our Mexico colleague will help you in your new case.

 

Kerry

 

 

View solution in original post

0 Kudos
12 Replies
806 Views
mdkhaledibnhassan
Contributor I

Hi I am trying to run "evkbmimxrt1170_lvgl_demo_widgets_cm7" without SDRAM but facing problem. It is a UI application. 
My question is: Is it possible to run "evkbmimxrt1170_lvgl_demo_widgets_cm7" or any scalable GUI/UI application without external RAM. 
For above configuration I am getting following errors:

../com.nxp.mcuxpresso.tools.win32_11.9.0.202307121226/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: evkbmimxrt1170_lvgl_demo_widgets_cm7.axf section `.bss_RAM2' will not fit in region `SRAM_ITC_cm7_user'

../com.nxp.mcuxpresso.tools.win32_11.9.0.202307121226/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: evkbmimxrt1170_lvgl_demo_widgets_cm7.axf section `.bss' will not fit in region `SRAM_ITC_cm7'

../com.nxp.mcuxpresso.tools.win32_11.9.0.202307121226/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: section .bss_RAM2 VMA [00030000,0023001f] overlaps section .bss VMA [00000440,003f5e57]

../com.nxp.mcuxpresso.tools.win32_11.9.0.202307121226/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: region `SRAM_ITC_cm7' overflowed by 3964504 bytes

../com.nxp.mcuxpresso.tools.win32_11.9.0.202307121226/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: region `SRAM_ITC_cm7_user' overflowed by 2031648 bytes

../com.nxp.mcuxpresso.tools.win32_11.9.0.202307121226/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: ./board/board.o: in function `BOARD_ConfigMPU':

Memory region Used Size Region Size %age Used

BOARD_FLASH: 575592 B 64 MB 0.86%

SRAM_ITC_cm7: 4161112 B 192 KB 2116.45%

SRAM_ITC_cm7_user: 2097184 B 64 KB 3200.05%

SRAM_DTC_cm7: 0 GB 256 KB 0.00%

SRAM_OC1: 0 GB 512 KB 0.00%

SRAM_OC2: 0 GB 512 KB 0.00%

SRAM_OC_ECC1: 0 GB 64 KB 0.00%

SRAM_OC_ECC2: 0 GB 64 KB 0.00%

collect2.exe: error: ld returned 1 exit status

make[1]: *** [makefile:117: evkbmimxrt1170_lvgl_demo_widgets_cm7.axf] Error 1

make: *** [makefile:108: all] Error 2

"make -r -j4 all" terminated with exit code 2. Build might be incomplete.

0 Kudos
797 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @mdkhaledibnhassan ,

  If you have any issues, please help to create your own question post, then we will help you in your own question post, don't just follow your question in the other customer's closed post, thanks a lot for your understanding.

Best Regards,

Kerry

0 Kudos
1,316 Views
ping1
Contributor V

Just tried and got an error in compiling like below:

ping1_0-1707144536098.png

Help is needed please.

Ping

 

0 Kudos
1,302 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @ping1 ,

  It's easy to realize it, please check the original project build result:

kerryzhou_0-1707198241754.png

We can see, the used SDRAM size is about 84KB, so, totally can put to the internal RAM.

Then, you can change the memory setting like this:

kerryzhou_1-1707198314049.pngkerryzhou_2-1707198391823.png

Then the new build result is:

kerryzhou_3-1707198418567.png

You can see, all the used data in the internal RAM now.

You can try it on your side.

BTW, you can remove XIP_BOOT_HEADER_DCD_ENABLE define to avoid the SDRAM definition:

kerryzhou_4-1707199833160.png

 

About your remove the SDRAM memory situation, it is mainly related to the board.c:

 

extern uint32_t __base_NCACHE_REGION;

extern uint32_t __top_NCACHE_REGION;

uint32_t nonCacheStart = (uint32_t)(&__base_NCACHE_REGION);

uint32_t size = (uint32_t)(&__top_NCACHE_REGION) - nonCacheStart;

 

You can change the memory also to the ITCM or DTCM, then you will build without any issues.

 

Wish it helps you!

Best Regards,

Kerry

 

 

 

 

0 Kudos
1,296 Views
ping1
Contributor V

Dear Kerry

Thanks for reply, followed and found an issue with it, in Managed Linker Script section configure the NonCacheable.init and NonCacheable to SRAM_ITC_cm7 will cause a failure in fsl_component_serial_manager.c at line 1245 - assert(handle), handle is in ITC memory location 0 and it stays there forever. Change to DTC and works

I have been caution to use ITC memory for variables, it caused issue for me in past when use RT1024, here is another one. Although this one can be solved by change the remove the assert(). My question is can we use ITC like DTC ? is it used by CPU for other tasks?

Another question about the board.c definition for nonCacheStart and size, look like we have to define a location for it? why?

Thank you!

Ping

 

0 Kudos
1,285 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @ping1 ,

   Thanks for your updated information.

   To the variables, it's better to put in the DTCM, as it is data TCM.

  If you want to use the ITCM, I think, maybe also can define some special area in the ITCM from the TOP side, not the 0 addres, just dived the ITCM into two pieces, then define your used area in your own defined TCM area.

  To the nonCacheStart, normally it is used for the SDRAM which need to use the nonCache area, as some SDK demo need to put the data in the noncache area for the SDRAM, you also can see the original area is indicated to the SDRAM area. So, we need to change it to the internal RAM when you don't use the external SDRAM.

  You can try it on your side.

  If you still have question about it, please kindly let me know.

Best Regards,

Kerry

0 Kudos
1,279 Views
ping1
Contributor V

Thanks for explanation, Kerry

Do you see the same issue in debug mode following the procedure as you showed? the serial handle ends up in ITC memory location 0, and it hangs.

Regards!

Ping

0 Kudos
1,276 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @ping1 ,

    You are welcome.

   Could you please also share one screenshot about serial handle ends up in ITC memory location 0?

  Then, I will test it on my side.

   Now, you want to use the ITCM, and it have issues, right? So, you use the DTCM instead of it, right?

 

Best Regards,

Kerry

0 Kudos
1,273 Views
ping1
Contributor V

Hi, Kerry

See the screen shot below, the Terminal window prints out Initializing PHY and then hangs at the location shown. If I change the both NonCacheable setting to SRAM_DTC_cm7 in Managed Linker Script , then no this issue, and it works fine, thanks. 

ping1_0-1707294689376.png

Regards!

Ping

0 Kudos
1,223 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @ping1 ,

  ITCM for NonCacheable setting also works on my side, please check my test result and the attached demo which I have written for you:

kerryzhou_0-1707400663526.png

kerryzhou_1-1707400671215.png

This is my DHCP test result:

kerryzhou_2-1707400688423.png

 

You can test it on your MIMXRT1170-EVK board.

Wish it helps you!

BTW, 2024 Chinese Spring Festival: Feb 9th to Feb 18th in total 10 days.
We will in the Spring Festival vacation, and back to work from 2.19th. During this time, you also can create the case, then our Mexico colleague will help you in your new case.

 

Kerry

 

 

0 Kudos
1,217 Views
ping1
Contributor V

Hi, Kerry

Thanks for trying, I see it works now because you create another section of SRAM_ITC_cm7_usr, which is not located on the memory address 0 location of ITC, otherwise it won't work, I will trying to do same in future if I need to use ITC too.

Happy Chinese New Year!

Regards!

Ping

 

966 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @ping1 ,

  You are always welcome!

   If you don't divide the specific area for your usr data, it may influence the original project requred ITCM area, that's why I define SRAM_ITC_cm7_usr.

  If you have any RT issues in the future, welcome to create the new question post to discuss it.

Best Regards,

Kerry

0 Kudos