How can I tune QSPI?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I tune QSPI?

1,421 Views
yongjin2712_cho
Contributor I

I'm using RT1050 mcu with MT25QL512 of micron.

I'm working well to read and erase and write to flash with SDR mode.

And MT25QL512 supports DDR mode. so I changes operation mode of flash from SDR to DDR

But in DDR mode, it doesn't work to read ID of flash

In SDR, I configure flexspi as below and it work well ( ID reads as 0x1020BA20)

flexspi_device_config_t deviceconfig = {
    .flexspiRootClk = 100000000,
    .flashSize = FLASH_SIZE,

     ...

}

CLOCK_InitUsb1Pfd(kCLOCK_Pfd0, 24);   /* Set PLL3 PFD0 clock 360MHZ. */
CLOCK_SetMux(kCLOCK_FlexspiMux, 0x3); /* Choose PLL3 PFD0 clock as flexspi source clock. */
CLOCK_SetDiv(kCLOCK_FlexspiDiv, 2);   /* flexspi clock 120M. */

const uint32_t customLUT[CUSTOM_LUT_LENGTH] = {

  [4 * NOR_CMD_LUT_SEQ_IDX_READID] =
   FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x9F, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04),
  [4 * NOR_CMD_LUT_SEQ_IDX_READID + 1] =
   FLEXSPI_LUT_SEQ(kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),

}

In DDR, I configure flexspi as below and it doesn't work well ( ID reads as 0x04882E08)

flexspi_device_config_t deviceconfig = {
    .flexspiRootClk = 45000000,
    .flashSize = FLASH_SIZE,

     ...

}

CLOCK_InitUsb1Pfd(kCLOCK_Pfd0, 24);   /* Set PLL3 PFD0 clock 360MHZ. */
CLOCK_SetMux(kCLOCK_FlexspiMux, 0x3); /* Choose PLL3 PFD0 clock as flexspi source clock. */
CLOCK_SetDiv(kCLOCK_FlexspiDiv, 3);   /* flexspi clock 90M. */

const uint32_t customLUT[CUSTOM_LUT_LENGTH] = {

  [4 * NOR_CMD_LUT_SEQ_IDX_READID] =
   FLEXSPI_LUT_SEQ(kFLEXSPI_Command_DDR, kFLEXSPI_1PAD, 0x9F, kFLEXSPI_Command_READ_DDR, kFLEXSPI_1PAD, 0x04),
  [4 * NOR_CMD_LUT_SEQ_IDX_READID + 1] =
   FLEXSPI_LUT_SEQ(kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),

}

How can I fix it?

0 Kudos
Reply
2 Replies

1,084 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you tell me if you set it to work in DTR mode?

Because I see that the memory needs to be configured for that, the Nonvolatile Configuration Register bit 5.

BR,

Aldo.

0 Kudos
Reply

1,084 Views
yongjin2712_cho
Contributor I

Ok, it needs some configuration to work in DTR mode as you said. So I'm trying to test it to set fifth bit of enhanced volatile configuration register

0 Kudos
Reply