Hello,
When I bring up custom board, I can't write firmware to flash memory (AT25SF128A).
And I can find "https://community.nxp.com/t5/i-MX-RT/RT1051-and-QSPI/m-p/795639".
With this, I execute "evkmimxrt1010_flexspi_nor_polling_transfer" at RAM with Debugger or openSDA.
I can fuse firmware to flash memory after that.
[Question]
Without debugger or OpenSDA, can I fuse firmware to flash memory but with only BootUtility(https://github.com/JayHeng/NXP-MCUBootUtility)?
Because it is hard to use debugger or OpenSDA at factory.
Thanks.
已解决! 转到解答。
Hello @emdev,
It looks like the issue is that by default the QE bit is not set by default, so you would need to set the respective Quad mode bit according to the memory that you're using:
Best Regards,
Alexis Andalon
Hello @emdev,
It looks like the issue is that by default the QE bit is not set by default, so you would need to set the respective Quad mode bit according to the memory that you're using:
Best Regards,
Alexis Andalon