Hard fault for 75% DTCM occupied

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hard fault for 75% DTCM occupied

Jump to solution
649 Views
Davidino
Contributor IV

Goodmorning,

I'm using a iMXRT1064 with SDK 1.11 and MCUExpresso 11.6.0.

The memory configuration is:

Senza titolo.png

The memory occupation is the following:

Memory region             Used Size Region Size %age Used
PROGRAM_FLASH:    555596 B  4 MB    13.25%
SRAM_DTC:                274208 B  384 KB 69.73%
SRAM_ITC:                  21328 B    128 KB 16.27%
SRAM_OC:                  26 KB        512 KB 5.08%

If I move the data from OCRAM (about 5% occupation) to DTCM (about 70% occupation) the program crashes. If I leave the data in OCRAM the program runs perfectly.

The data that occupies 26kB is a single array of struct.

What are the possible reasons why the program crashes despite not having overflow 100% of memory occupation?

In attachment the .map file of my project.

Thank you.

Labels (1)
0 Kudos
1 Solution
617 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @Davidino ,

The FlexRAM settings seems fine. I also test on my board, it can work. I can write data to 0x20077000, but can't write to 20079000. So, it works.

 

Regards,

Jing

View solution in original post

4 Replies
633 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @Davidino ,

Maybe there is some bugs in application, like stack overflow.

 

Regards,

Jing

0 Kudos
630 Views
Davidino
Contributor IV

Hello @jingpan ,

thank you for your answer.

Below you can find the stack and heap usage in the working project, at full operation: 

dasasd.png

And here the stack and heap usage in the NOT working project, when the error triggers: 

Davidino_2-1669630916160.png

If the problem was the stack overflow, I think that it would be visible here.

Since the project is very complex, I propose an hypothetichal cause for the error.

Following the link: https://community.nxp.com/t5/i-MX-RT/How-to-reconfigure-the-flexRAM-on-i-mxRT-1062-using-MCUXpresso/... , I reconfigured the FlexRam in run time with the following modifications and below I highlight the most significant changes:

gdfgfdgdfgdfgdfgd.png

fgdfsggfdssfdfsdsfdsfd.png

The code at startup is:

 

__attribute__ ((section(".after_vectors.reset")))
void ResetISR(void) {

    // Disable interrupts
    __asm volatile ("cpsid i");

    /* Reallocating the FlexRAM */
     __asm (".syntax unified\n"

    		 "LDR R0, =0x20003fff\n"	// load initial value to stack pointer into R0
    	     "MSR MSP,R0\n"				// re-initialize stack pointer by new value

    		 "LDR R0, =0x400ac044\n"	// Address of register IOMUXC_GPR_GPR17
    		 	 	 	 	 			// Modificato rispetto all'originale per rispettare la configurazione via eFuses
    		 //"LDR R1, =0x5AAFFAA5\n"	// FlexRAM configuration DTC = 256KB, ITC = 128KB, OC = 128KB
    		 //"LDR R1, =0xAAAFFAAA\n"	// FlexRAM configuration DTC = 384KB, ITC = 128KB, OC = 0KB
    		 "LDR R1, =0xEAAAAAAA\n"	// FlexRAM configuration DTC = 480KB, ITC = 32KB, OC = 0KB
    		 "STR R1,[R0]\n"

    		 "LDR R0,=0x400ac040\n"		// Address of register IOMUXC_GPR_GPR16
    		 "LDR R1,[R0]\n"
    		 "ORR R1,R1,#4\n"			// The 4 corresponds to setting the FLEXRAM_BANK_CFG_SEL bit in register IOMUXC_GPR_GPR16
    		 "STR R1,[R0]\n"
...

 

And the MPU configuration is:

 

    /* Region 0 setting: Instruction access disabled, No data access permission. */
    MPU->RBAR = ARM_MPU_RBAR(0, 0x00000000U);
    MPU->RASR = ARM_MPU_RASR(1, ARM_MPU_AP_NONE, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_4GB);

    /* Region 1 setting: Memory with Device type, not shareable, non-cacheable. */
    MPU->RBAR = ARM_MPU_RBAR(1, 0x80000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_512MB);

    /* Region 2 setting: Memory with Device type, not shareable,  non-cacheable. */
    MPU->RBAR = ARM_MPU_RBAR(2, 0x60000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_512MB);

#if defined(XIP_EXTERNAL_FLASH) && (XIP_EXTERNAL_FLASH == 1)
    /* Region 3 setting: Memory with Normal type, not shareable, outer/inner write back. */
    MPU->RBAR = ARM_MPU_RBAR(3, 0x70000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_RO, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_4MB);
#endif

    /* Region 4 setting: Memory with Device type, not shareable, non-cacheable. */
    MPU->RBAR = ARM_MPU_RBAR(4, 0x00000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_1GB);

    /* Region 5 setting: Memory with Normal type, not shareable, outer/inner write back */
    MPU->RBAR = ARM_MPU_RBAR(5, 0x00000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_32KB);		// ITCM

    /* Region 6 setting: Memory with Normal type, not shareable, outer/inner write back */
    MPU->RBAR = ARM_MPU_RBAR(6, 0x20000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_512KB);		// DTCM

    /* Region 7 setting: Memory with Normal type, not shareable, outer/inner write back */
    MPU->RBAR = ARM_MPU_RBAR(7, 0x20200000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_512KB);		// OCRAM

    /* Region 8 setting: Memory with Normal type, not shareable, outer/inner write back */
    //MPU->RBAR = ARM_MPU_RBAR(8, 0x20280000U);
    //MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_512KB);

    /* Region 11 setting: Memory with Device type, not shareable, non-cacheable */
    MPU->RBAR = ARM_MPU_RBAR(11, 0x40000000);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_4MB);

    /* Region 12 setting: Memory with Device type, not shareable, non-cacheable */
    MPU->RBAR = ARM_MPU_RBAR(12, 0x42000000);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_1MB);

    /* Enable MPU */
    ARM_MPU_Enable(MPU_CTRL_PRIVDEFENA_Msk);

    /* Enable I cache and D cache */
    SCB_EnableDCache();
    SCB_EnableICache();
...

 

If you think that this changes are fine, I close the topic as it's too difficult via chat to examine anything.

Thank you in advanced.

Regards,

Davidino

 

0 Kudos
618 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @Davidino ,

The FlexRAM settings seems fine. I also test on my board, it can work. I can write data to 0x20077000, but can't write to 20079000. So, it works.

 

Regards,

Jing

613 Views
Davidino
Contributor IV

Hello @jingpan ,

thank you for your answer and confirmation. For the moment I found a work-around using OCRAM, in the future I'll dig deeper what may be the cause of the problem.

Thank you again.

0 Kudos