FlexSPI Boot - which FlexSPI port?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FlexSPI Boot - which FlexSPI port?

892 次查看
chriscowdery
Contributor V

Hi All,

 According to the reference manual for iMXRT1021, table 8-1 (ROM Bootloader Peripheral PinMux), the Bootloader can boot from FlexSPI_A in two places, and FlexSPI_B.

But I cannot see how it decides which one is the correct port?

Does it try all of them until it finds a good one?

I see nothing in the fuses or GPIO pins to control this feature?


Thanks,


Chris.

标签 (1)
标记 (3)
3 回复数

793 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Chris, 

ROM does not support boot from FLEXSPI_B port directly. ROM always seeks a valid Flash Configuration Block from the FLEXSPI_A port and then re-configures the FLEXSPI controller using the valid parameters in the block read-out. This reconfiguration can include but is not limited to, FLEXSPI_B port support.

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------- 

793 次查看
chriscowdery
Contributor V

Hi Victor,

 Thanks. Does that also mean that the Boot ROM always uses FLEXSPI_A 'primary pinmux' ? I.e. I cannot connect my Flash to the 'secondary pinmux' port (page 186 of Reference Manual) ?

Thanks,

Chris.

793 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Chris,

 

You can use the secondary pinmux, but keep in mind that these pins are used only for QSPI devices as specified in Table 8-9. Also, if you want to use these pins you will have to burn the corresponding fuses on the BOOT_CFG1 field.

Regards, 

Victor