Flashing bootloader ,bootstrap and application binaries via serial downloader mode using Ivaldi tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing bootloader ,bootstrap and application binaries via serial downloader mode using Ivaldi tool

391 Views
jnj
Contributor III

Hi All,

I could flash boot loader ,bootstrap and application binaries using Ivaldi tool and serial down loader method.But once device is flashed using this method , for next flashing binary using jlink is causing some issues in the NXP . We are not able to access nxp via usb console after flashing . What could be the reason for this?Kindly help us to resolve the issue.

0 Kudos
1 Reply

381 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @jnj ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

   After you: flash boot loader ,bootstrap and application binaries using Ivaldi tool and serial down loader method

 Whether the code function works or not after switch to the internal boot mode?

  When you debugger meet the can't boot issues, normally, it is caused by the invalid image, but, it is easy to resolve it, just do the mass erase, if you still have issues, you also can enter the serial download mode do the mass erase, then JLINK should can debug it again.

 

Wish it helps you!

Best Regards,

kerry

0 Kudos