FOTA using ethernet or MQTT in IMXRT1064

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FOTA using ethernet or MQTT in IMXRT1064

927件の閲覧回数
karthik1
Contributor I

1.Any API to do operation on internal flash  in IMXRT1064?

1.Please suggest me the approach to do FOTA update using Ethernet (application program to download the firmware  into external flash hyperflash/ QSPI NOR flash )  in imxRT1064 board.?

2.Amazon FreeRTOS  OTA demo code is supported for imxRT1060 but not given SDK Amazon FreeRTOS  OTA demo code for imxRT1064 ,is it available for IMXRT1064 board?

3. Any suggestion using secondary bootloader to do FOTA?

 

タグ(3)
0 件の賞賛
1 返信

822件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

This is a duplicated thread. Please refer to this post: https://community.nxp.com/thread/522713 

0 件の賞賛