Error in IMXRT1050-EVKB ( and 1060 ) schematic, ethernet

cancel
Showing results forย 
Search instead forย 
Did you mean:ย 

Error in IMXRT1050-EVKB ( and 1060 ) schematic, ethernet

281 Views
gpontis
Contributor IV

There appears to be a design error in the ethernet circuit on the IMXRT1050-EVKB and MIMXRT1060-EVK. Both show 49.9 ohm terminating resistors R126 through R129 on RXP, RXN, TXP, and TXN. However, the KSZ8081RNB PHY has internal termination. The Microchip hardware design guide for this chip ( DS00002779A ) says of all four of these lines:

It has an internal terminator and a bias, so it can be directly connected to the transmit channel of the magnetics and no external terminator and bias are needed

Adding the resistors would double-terminate the lines, but it would not be surprising if ethernet still worked under good conditions. Problems would be most likely to show up with longer cables.

On a related note, the eval boards also show places to optionally install 4 capacitors, one per line. These are marked DNP. I cannot think of any situation where these caps would be desired, so better to save the PCB board area and leave them off.

George

1 Reply

93 Views
nxf46838
NXP TechSupport
NXP TechSupport

Hello George,

Thank you for your review, we are grateful of your comments about it, we will review it,

Best Regards,

Aldo

0 Kudos