Enable ETM trace on IMXRT1052

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable ETM trace on IMXRT1052

1,005件の閲覧回数
michaelsmith
Contributor I

How to enable ETM trace on IMXRT1052 processor using Keil ARM MDK?  What registers (e.g. IOMUXC, CCM, etc) need to be configured to output the trace data.  How to set up the debug/trace dialog in Keil IDE?

0 件の賞賛
1 返信

794件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Michael,

According with section 7.2.2.3 “Embedded Trace Macrocell (ETM)” of i.MXRT1052 Reference Manual, in case of requiring information about ETM, it is required referring to “ARM® CoreSight™ ETM-M7 Revision r0p1 Technical Reference Manual” document (link below), as it is part of the ARM debug features:

https://static.docs.arm.com/ddi0494/b/DDI0494.pdf

Additionally, you also need to ensure that you have a proper debug tool that supports ETM features, like the Segger J-Trace:

https://www.segger.com/products/debug-probes/j-trace/


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛