Hi,
I am trying to test SDK ecompass application on evk i.MX RT1010 kit.
Seems that the sensor is not detected;
The error message:
. Sensor device initialize failed!
Ok, that's the root problem, so you can find one FXOS8700 and solder it to your board, check the external circuit, then the code should work on your side.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
ecompss project in the SDK need to use the on board FXOS8700 sensor, so, please check your board, do you have the U26 on board COMBO SENSOR chip?
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Eric Williams,
The board didn't contains FXOS8700 , it is caused by the out of stock when manufacture the MIMXRT1010-EVK board.
So, now, you can buy the FXOS8700 and solder it by yourself.
Best Regards,
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Eric Williams,
As I know, MIMXRT1050-evkb contains this component, but MIMXRT1060-EVK and MIMXRT1010-EVK don't contains this component, just contains the package.
So, the customer may need to buy or apply the sample about this chip from the NXP website.
About the question: Are they intended to be populated?
Maybe not, but I already help you to check it with our hardware department, any reply will let you know.
Best Regards,
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------