RT1050 seems to support Zephyr OS, but there is no explanation for other Linux, so it seems to be unsupported.
Does the RT1050 support Linux or RTOS?
If you apply, are there any pages or resources that you can refer to for porting?
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Does the RT1050 support Linux or RTOS?
-- A variety of RTOS are available to be deployed on i.MX RT series MCU, however, it's impossible to run the Linux.
NXP has provided some FreeRTOS demo project in the SDK library, then developers can refer to them for details.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------