Is there a solid example of setup and use of the systick for the 1050evbk thanks.
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you refer to the iled_blinky demo which resides ~\boards\evkbimxrt1050\demo_apps\led_blinky of SDK library, as the demo shows how to use the systick timer.
Further, the download link of the SDK library for the MIMXRT1050 is attached below.
https://mcuxpresso.nxp.com/en/welcome
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------